I have returned your license, when you re-activate, the new expiration date will be loaded.
Best Regards,
Mike
Dear Mike,
I installed the S32 Design Studio for S32 Platform, it shows my license expiring.
Because I didn't get a valid license to install Extensions and Updates.
I had refresh, but it still fail.
I also check my license on the NXP.com website, but it shows Expiration Data is 2026/4/6
Hi,
I'm not sure what's the issue - if you stretch a little bit the column with Message License Expiring... you will probably see something like this:
Means your license will expire after 4 years.
What particular issue do you have - can you please share a screenshot with error message? Which update/package you can't install?
Jiri
Hi Mike:
can you also help to return my license,thanks!
License Applicable to Product(s): Version Description 2.2 S32 Design Studio for ARM v2.2
License Quantity: 1
Fulfillment ID: 175776437
Expiration Date: Jul 29, 2021
Product: S32 Design Studio for ARM v2.2
Machine: CF30D5D79DD2230677821310B765396A863F0550 Activation
Code: 919B-D4D4-4E64-0434
Hi Bevan,
Your entitlement expiration is in 2025, probably you just need to refresh the license in S32 Design Studio. Also, you could return the license and re-activate. Sometimes it's not possible to do either. If this is the case for you, I can return the license on the server side. Just let me know.
Best Regards,
Mike
Hi mike.
Can you also refresh my license for S32 Design Studio for ARM 2.2 ?
License Quantity: 1
Expiration Date: Jul 6, 2021
Code: 01D6-1D4C-0851-E4A9
I can't return the license, and it is not possible to re-install this software again.
Or, let me know how to re-activate the license.
Best regards.
Can I get my license renewed for S32 Design Studio for ARM 2.2
The license has expired.
Thanks,
Stephan
Hello @stephandewit1,
I have returned your expired license, but the entitlement was already extended. Just re-activate with same activation code and you will receive a new license.
Best regards,
Mike
I have the same problem. Can you please re-activate my licence?
Fulfillment ID: 152126887
Expiration Date: Nov 7, 2021
Product: S32 Design Studio for PA E200
Machine: CB93635434074A5B26076ED3A12D8E2F204A0001
Activation Code: 9441-28CA-C473-A597
Hello @jackeyhong ,
I have returned your license on the server, please re-activate the same activation code you already have. It will then show the new expiration date.
Best Regards,
Mike