Hello Team,
I started using S32 Design studio from few days.
currently I am working on S32K142 microcontroller for sound application.
When I try to configure any peripheral from Peripheral Option , It is showing that Peripheral not present in toolchain project. If I select All available component then it is giving below warning.
Below are some details of project.
Please help me with explaining what to do in steps.
Thanks!
Hi MohitManvar,
According to the "6.3 Compiler and IDE versions" of S32SDK_for_S32K1xx_RTM_4.0.1_ReleaseNotes.pdf:
GreenHills compiler v. 2017.1.4
IAR compiler v. 8.11.2
GCC compiler for ARM v. 6.3.1 20170509
Wind River Diab Compiler v5.9.6.2
ARM Compiler 6.6.1 Long Term Maintenance
S32 Design Studio 3.3 IDE
Do not use S32DS v3.5, please use S32DS v3.4+S32K1 SDK RTM4.0.3.
Sorry for the inconvenience we bring you!
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------