LpuartFlexio_Uart_Ip_Example_S32K344 with interrupt not working

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LpuartFlexio_Uart_Ip_Example_S32K344 with interrupt not working

620 次查看
janakiraman-s
Contributor I

Hi Team,

I am currently using the LpuartFlexio_Uart_Ip_Example_S32K344 example code. I made some changes to enable simple transmission and reception from UART with interrupt mode. While the transmission is working perfectly, I am facing an issue with the reception side. The callback function gets triggered only once. When I send data a second time, the callback function does not get triggered.

"Could you please assist me in resolving this problem?"

 

Thanks,

Janakiraman

0 项奖励
回复
2 回复数

301 次查看
Vamsi421
Contributor II

I am also facing same problem. If your problem is solved then help me how to solve this.

thanks

 

0 项奖励
回复

586 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Janakiraman,

Seems that you forget call Lpuart_Uart_Ip_SetRxBuffer() in LPUART_UART_IP_EVENT_RX_FULL  of rx callback. Please refer to the discussion in: UART_Lpuart_Uart_Ip_AsyncReceive_loss_packet


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复