Installation of S32DS.3.4_b201217_win32.x86_64 rolling back

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Installation of S32DS.3.4_b201217_win32.x86_64 rolling back

1,824件の閲覧回数
bvikas
NXP Employee
NXP Employee

Installation of S32SD3.4 is not completing. It is rolling back before asking for Activation code.

Please find attached the logs.

Thanks

0 件の賞賛
返信
8 返答(返信)

1,776件の閲覧回数
bvikas
NXP Employee
NXP Employee

Hi All,

We need to get Local Admin rights to install S32 Design Studion V-3.4 and V3.5

0 件の賞賛
返信

1,808件の閲覧回数
bvikas
NXP Employee
NXP Employee

I am running as Admin
But still the same issue.

0 件の賞賛
返信

1,794件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

Hello,

As an NXP employee, please start 'Admin by Request' session AND use the 'Run as Administrator' option from the right-click menu on the installer. It seems sometimes the admin status is not functioning as expected and this procedure has worked for some NXP users.

Best Regards,

Mike

0 件の賞賛
返信

1,777件の閲覧回数
bvikas
NXP Employee
NXP Employee

Hello Mike,

These steps are also not working.

0 件の賞賛
返信

1,750件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

Hello @bvikas,

We recently discussed the issue with NXP IT. They recommend using the option 'Windows 7 compatibility mode' when installing S32 Design Studio to avoid the admin rights issue. Please try this and let us know if it resolves your issue.

Best Regards,

Mike

0 件の賞賛
返信

1,772件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

Hello,

I think you need to contact IT, please submit a SNOW ticket to get this resolved. It could be the access setup for your account on your PC which are different in some way to cause you more difficulty than other NXP users.

Mike

0 件の賞賛
返信

1,815件の閲覧回数
hanraaijmakers
NXP Employee
NXP Employee

run as admin

0 件の賞賛
返信

1,816件の閲覧回数
hanraaijmakers
NXP Employee
NXP Employee

We have the same problem.

0 件の賞賛
返信