Installation of S32DS.3.4_b201217_win32.x86_64 rolling back

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Installation of S32DS.3.4_b201217_win32.x86_64 rolling back

1,821 次查看
bvikas
NXP Employee
NXP Employee

Installation of S32SD3.4 is not completing. It is rolling back before asking for Activation code.

Please find attached the logs.

Thanks

0 项奖励
回复
8 回复数

1,773 次查看
bvikas
NXP Employee
NXP Employee

Hi All,

We need to get Local Admin rights to install S32 Design Studion V-3.4 and V3.5

0 项奖励
回复

1,805 次查看
bvikas
NXP Employee
NXP Employee

I am running as Admin
But still the same issue.

0 项奖励
回复

1,791 次查看
mikedoidge
NXP Employee
NXP Employee

Hello,

As an NXP employee, please start 'Admin by Request' session AND use the 'Run as Administrator' option from the right-click menu on the installer. It seems sometimes the admin status is not functioning as expected and this procedure has worked for some NXP users.

Best Regards,

Mike

0 项奖励
回复

1,774 次查看
bvikas
NXP Employee
NXP Employee

Hello Mike,

These steps are also not working.

0 项奖励
回复

1,747 次查看
mikedoidge
NXP Employee
NXP Employee

Hello @bvikas,

We recently discussed the issue with NXP IT. They recommend using the option 'Windows 7 compatibility mode' when installing S32 Design Studio to avoid the admin rights issue. Please try this and let us know if it resolves your issue.

Best Regards,

Mike

0 项奖励
回复

1,769 次查看
mikedoidge
NXP Employee
NXP Employee

Hello,

I think you need to contact IT, please submit a SNOW ticket to get this resolved. It could be the access setup for your account on your PC which are different in some way to cause you more difficulty than other NXP users.

Mike

0 项奖励
回复

1,812 次查看
hanraaijmakers
NXP Employee
NXP Employee

run as admin

0 项奖励
回复

1,813 次查看
hanraaijmakers
NXP Employee
NXP Employee

We have the same problem.

0 项奖励
回复