I have imported a project in S32DS but the scr folder is empty

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I have imported a project in S32DS but the scr folder is empty

446 Views
hanhan
Contributor I

I have imported a project in S32DS but the src folder is empty,as shown in the picture below:

hanhan_0-1676986633173.png

The project src folder I imported had something in it, as follows:

hanhan_1-1676986734518.png

Can you engineers see if you can help me out?

 

 

 

0 Kudos
Reply
1 Reply

431 Views
mikedoidge
NXP Employee
NXP Employee

Hello @hanhan,

In the image you attached, I can see you are looking at the 'Build Targets' view. This view filters the project contents for items which are Build Targets. Since there are no Build Targets in the 'src' folder, it will show as empty.

I suggest you look to the 'Project Explorer' view to see the contents of the project, including the source files in the 'src' folder.

Best Regards,

Mike

0 Kudos
Reply