I have installed the S32K3 Design Studio 3.5 (using S32DS.3.5_b220726_win32.x86_64.exe) in my notebook and encountered activation issue as below. The installation could not complete after the message had popped up. My notebook is with Windows 10. Tried both online & offline activation.
online error message as below
"Error sending an activation request to a remote activation server and processing the resulting response. That activation request yields no right to a license.(FNP error 0)"
offline activation.xml as below
"Response xmlns="http://www.macrovision.com/fnp/2004/11/activation"
"
How can I activate S32DS.3.5 successfully?
已解决! 转到解答。
Hi, @Niukk ,
Please can you check this troubleshooting guide : https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/Troubleshooting-Activation-fails-with-...
If it is still not working please can you share the log from
S32DS installation path :
C:\NXP\S32DS.3.5\_S32 Design Studio for S32 Platform 3.5_installation\Logs
Thank you,
Best regards.
- Mehul Patel
Hi,
i prepare to install s32ds3.5 and try to use a normal activate code to register it, but it is fail. This information is "errorNo=21, errorString=Error sending an activation request to a remote activation server and processing the resulting response. The quantity specified exceeds maximum quantity allowed (0). (FNP error 0), flxActMajorErrorNo=0, flxActMinorErrorNo=0, flxActSysErrorNo=0, flxCommErrorNo=0"
i also try to use "CLL_FNP.11.18.0.2.zip and Activation.7z", but there are some error below. please help to check it. thanks.
java -Djava.library.path="{C:/Users/mei98/Downloads}/Activation/cll/x64" -jar "{C:/Users/mei98/Downloads}/Activation/license.jar" activateUI
Error: Unable to access jarfile {C:/Users/mei98/Downloads}/Activation/license.jar