Hi NXP,
I am trying to use C code to test SMR install API(service ID:
), However, I always got service response A5AAA399 which meas parameter is incorrect.
there is so many Argument in this API, could someone help me to check?
the signature and address have benn vailded is this test.
the HSE FW version is 0.2.6
memcpy(
(void *)&IVT,
(const void *)BLOCK0_IVT_ADDRESS,
0x100);
uint32_t AppAddress = (uint32_t) app_start_real;
SmrEntry[4].pSmrsrc=AppAddress; /* Start of APP code */
SmrEntry[4].smrSize = 1024UL; /* Length of APP code */
SmrEntry[4].authKeyHandle = aaa_pub_HANDLE;
SmrEntry[4].authScheme.sigScheme.signSch = HSE_SIGN_RSASSA_PSS;
SmrEntry[4].authScheme.sigScheme.sch.rsaPss.hashAlgo = HSE_HASH_ALGO_SHA2_256;
SmrEntry[4].authScheme.sigScheme.sch.rsaPss.saltLength = 32UL;
SmrEntry[4].pInstAuthTag[0] = test_sign_real; /* signature tag address */
SmrEntry[4].pInstAuthTag[1] = (uint32_t)NULL; /* In this example, AES keys is used hence 2nd tag address is NULL */
/**** RSA ****/
srvResponse = RsaPssSignSrv(
aaa_pri_HANDLE,
32UL,
HSE_HASH_ALGO_SHA2_256,
SmrEntry[4].smrSize,
(const uint8_t *)SmrEntry[4].pSmrSrc,
FALSE,
0U,
&signLength,
outputSig);
debug_print("%s RsaPssSignSrv(1) = %x\r\n", sl_tag, srvResponse);
if(FLASH_Erase(FLS_SWAP_OFFSET, S32K312_SECTOR_SIZE, MAX_ERASE_TIME) == E_OK){
if(FLASH_Write(FLS_SWAP_OFFSET, sizeof(outputSig), outputSig, MAX_ERASE_TIME) == E_OK){
debug_print("%s FLASH_Write = OK\r\n", sl_tag);
}
else{
debug_print("%s FLASH_Write = NG\r\n", sl_tag);
}
}
else{
debug_print("%s FLASH_Erase = NG\r\n", sl_tag);
}
srvResponse = RsaPssVerSrv(
aaa_pub_HANDLE,
32UL,
HSE_HASH_ALGO_SHA2_256,
SmrEntry[4].smrSize,
(const uint8_t *)SmrEntry[4].pSmrSrc,
FALSE,
0U,
&signLength,
(const uint8_t *)test_sign_real);
debug_print("%s RsaPssVerSrv(1) = %x\r\n", sl_tag, srvResponse);
srvResponse = HSE_InstallSmrEntry((4),
(const hseSmrEntry_t *)&SmrEntry[4],
(const uint8_t *)SmrEntry[4].pSmrSrc,
SmrEntry[4].smrSize,
(const uint8_t *)tag_addr[0][4],
(const uint8_t *)tag_addr[1][4],
tag_len[4],
tag_len[4]);
debug_print("%s HSE_InstallSmrEntry(0) = %x\r\n", sl_tag, srvResponse);
And, here is result.
Also, I refer to demo_app\services\src\secure_boot\hse_secure_boot.c which is below(Snippet)
srvResponse = HSE_InstallSmrEntry((Index),
(const hseSmrEntry_t *)&smrEntry[Index],
(const uint8_t *)smrEntry[Index].pSmrSrc,
smrEntry[Index].smrSize,
(const uint8 *)tag_addr[0][Index],
(const uint8 *)tag_addr[1][Index],
tag_len[Index],
tag_len[Index]);
smrEntry[i].configFlags = HSE_SMR_CFG_FLAG_INSTALL_AUTH; /* Indicate that verification should be done on provided signature */
smrEntry[i].pSmrDest = 0U; /* destination address shall be NULL for flashed based devices */
smrEntry[i].checkPeriod = 0U;
smrEntry[i].pSmrsrc=AppAddress; /* Start of APP code */
smrEntry[i].smrSize = 1024UL; /* Length of APP code */
smrEntry[i].authKeyHandle = HSE_DEMO_NVM_RSA2048_PUB_CUSTAUTH_HANDLE0;
smrEntry[i].authScheme.sigScheme.signSch = HSE_SIGN_RSASSA_PSS;
smrEntry[i].authScheme.sigScheme.sch.rsaPss.hashAlgo = HSE_HASH_ALGO_SHA2_256;
smrEntry[i].authScheme.sigScheme.sch.rsaPss.saltLength = SALT_LENGTH;
smrEntry[i].pInstAuthTag[0] = RSA_TAG_CODE_FLASH_ADDRESS; /* signature tag address */
smrEntry[i].pInstAuthTag[1] = (uint32_t)NULL; /* In this example, AES keys is used hence 2nd tag address is NULL */
Hi @lukaszadrapa,
Thanks for reply,
sorry for missing definition of argument. this parameter(test_sign_real) is follow on demo code(hse_secure_boot.c), here is the definitions
My test code
#define app_start_real 0x500000UL
#define test_sign_real 0x440000UL
#define test_HANDLE GET_KEY_HANDLE(HSE_KEY_CATALOG_ID_NVM,3,0)
static const uint32_t tag_addr[2U][5U] =
{
{0, 0, 0, 0, test_sign_real},
{0, 0, 0, 0, 0}};
static const uint32_t tag_len[] =
{
16U, 16U, 16U, 32U, 512U};
demo code(hse_secure_boot.c)
#define RSA_TAG_CODE_FLASH_ADDRESS 0x00454100UL
static const uint32_t tag_addr[2U][5U] =
{
{CMAC_TAG_CODE_FLASH_ADDRESS, GMAC_TAG_CODE_FLASH_ADDRESS, HMAC_TAG_CODE_FLASH_ADDRESS, ECC_TAG1_CODE_FLASH_ADDRESS, RSA_TAG_CODE_FLASH_ADDRESS},
{0, 0, 0, ECC_TAG2_CODE_FLASH_ADDRESS, 0}};
static const uint32_t tag_len[] =
{
16U, 16U, 16U, 32U, 256U};
Basically, It's the same except the value.
I try demo code in Trace32, and it's work, but I still don't know the different between my test code and demo code...
Hi @JasonChou
One more thing that comes into my mind - most of similar issues when it does not work in own project is caused by cache memory.
It is important to force descriptors/data sent to/from Messaging Unit to non-cacheable region. To check if it is related to the cache memory, you can try to disable the cache by DC bit in core register CCR Configuration and Control Register. Please let me know if it helps or not.
Regards,
Lukas
Hi @JasonChou
it's core registers, so it's described in the core manuals:
http://infocenter.arm.com/help/index.jsp?topic=/com.arm.doc.ddi0489d/index.html
http://infocenter.arm.com/help/index.jsp?topic=/com.arm.doc.dui0646b/index.html
hseSmrEntry_t (your SmrEntry[4]) has more items which I can't see in the code. You can find details in API RM. Could you check how those items are initialized?
And maybe you can take a look also at these examples:
https://www.nxp.com/webapp/Download?colCode=S32K3_HSE_DemoExamples
This one could help:
c:\NXP\S32K3_HSE_DemoExamples_1_0_0\S32K3_HSE_DemoExamples\Secure_Boot\S32K344_Advanced_SecureBoot\
Regards,
Lukas
Hi @JasonChou
SmrEntry[4].pInstAuthTag[0] = test_sign_real; /* signature tag address */
This should be a pointer to the signature only, not directly the value. Could you check this?
Thanks,
Lukas