Does S32DS have a example project for MPC5644A PIT interrupt?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Does S32DS have a example project for MPC5644A PIT interrupt?

跳至解决方案
1,348 次查看
alexhuang5367
Contributor II

Just like the title

Could any one provide a S32DS example for MPC5644A PIT interrupt.

I have this requirement because when i use CW2.1 my project is able to work, but turn to S32DS i can't open the interrupt 

when i open interrupt S32DS IDE just "Program received signal SIGTRAP, Trace/breakpoint trap.
0x00000004 in RCHW2 ()"

 

Please every one

标签 (1)
标记 (3)
0 项奖励
1 解答
1,163 次查看
martin_kovar
NXP Employee
NXP Employee

Hi,

I described the problem to your previous thread.

MPC5644A mounted on S32DS can not open interrupt S32DS is a big bug IDE? 

Here is the fixed project, which should work. Please try and let me know, if it works.

Regards,

Martin

在原帖中查看解决方案

0 项奖励
1 回复
1,164 次查看
martin_kovar
NXP Employee
NXP Employee

Hi,

I described the problem to your previous thread.

MPC5644A mounted on S32DS can not open interrupt S32DS is a big bug IDE? 

Here is the fixed project, which should work. Please try and let me know, if it works.

Regards,

Martin

0 项奖励