Can you provide me with relevant hardware information about S32R274RRUEVB, such as pin name, pin attribute type, PCB package size data?thank you

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can you provide me with relevant hardware information about S32R274RRUEVB, such as pin name, pin attribute type, PCB package size data?thank you

1,850 Views
shiyu
Contributor I


Can you provide me with relevant hardware information about S32R274RRUEVB, such as pin name, pin attribute type, PCB package size data?thank you

0 Kudos
9 Replies

1,635 Views
jiri_kral
NXP Employee
NXP Employee

Hello, 

You can get more details on product page S32R274 Radar Microcontroller Evaluation Board|NXP  

Jiri

0 Kudos

1,634 Views
shiyu
Contributor I

Hello

I can't find the information I need on the S32R274 radar microcontroller evaluation board, can you provide the information I need?It's better to describe it visually, thank you

shi

国内首家EPB电子刹车量产企业

The first EPB electronic brake mass production enterprises

浙江力邦合信智能制动系统股份有限公司 石煜 ShiYu

Zhejiang Libang Hexin Intelligent Brake System Co., Ltd.

MOB:15869637318

Postal code:325400

EMAIL: shiyu@cnlbn.com

TEL:0577-63171555

ADD:浙江省平阳万全轻工基地兴隆路111号

No.111, Xinglong Road, Wanquan Light Industrial Zone,

Pingyang County, Zhejiang Province, China.

HTTP:WWW.CNLBN.COM

发件人: jiri.kral@nxp.com

发送时间: 2017-11-28 15:44

收件人: 煜 石

主题: Re: - Re: Can you provide me with relevant hardware information about S32R274RRUEVB, such as pin name, pin attribute type, PCB package size data?thank you

NXP Community

Re: Can you provide me with relevant hardware information about S32R274RRUEVB, such as pin name, pin attribute type, PCB package size data?thank you

reply from Jiri Kral in S32 Design Studio - View the full discussion

Hello,

You can get more details on product page S32R274 Radar Microcontroller Evaluation Board|NXP

Jiri

Reply to this message by replying to this email, or go to the message on NXP Community

Start a new discussion in S32 Design Studio by email or at NXP Community

Following Re: Can you provide me with relevant hardware information about S32R274RRUEVB, such as pin name, pin attribute type, PCB package size data?thank you in these streams: Inbox

This email was sent by NXP Community because you are a registered user.

You may unsubscribe instantly from NXP Community, or adjust email frequency in your email preferences

0 Kudos

1,634 Views
jiri_kral
NXP Employee
NXP Employee

Hi Shi, 

You can find EVB board schematic here - https://www.nxp.com/downloads/en/schematics/S32R274-SPF.pdf 

And more details in EVB user guide - https://www.nxp.com/docs/en/user-guide/S32R274-EVBUG.pdf 

Jiri

0 Kudos

1,633 Views
shiyu
Contributor I

Hi Jiri,

I do find the name information of the symbol pin from the information you gave, but there is no information about the type of pins, and there is no information about PCB packaging.

Can you provide it?I've been on the NXP website for a long time to come to you for help

Shi

国内首家EPB电子刹车量产企业

The first EPB electronic brake mass production enterprises

浙江力邦合信智能制动系统股份有限公司 石煜 ShiYu

Zhejiang Libang Hexin Intelligent Brake System Co., Ltd.

MOB:15869637318

Postal code:325400

EMAIL: shiyu@cnlbn.com

TEL:0577-63171555

ADD:浙江省平阳万全轻工基地兴隆路111号

No.111, Xinglong Road, Wanquan Light Industrial Zone,

Pingyang County, Zhejiang Province, China.

HTTP:WWW.CNLBN.COM

发件人: jiri.kral@nxp.com

发送时间: 2017-11-28 16:05

收件人: 煜 石

主题: Re: - Re: Can you provide me with relevant hardware information about S32R274RRUEVB, such as pin name, pin attribute type, PCB package size data?thank you

NXP Community

Re: Can you provide me with relevant hardware information about S32R274RRUEVB, such as pin name, pin attribute type, PCB package size data?thank you

reply from Jiri Kral in S32 Design Studio - View the full discussion

Hi Shi,

You can find EVB board schematic here - https://www.nxp.com/downloads/en/schematics/S32R274-SPF.pdf

And more details in EVB user guide - https://www.nxp.com/docs/en/user-guide/S32R274-EVBUG.pdf

Jiri

Reply to this message by replying to this email, or go to the message on NXP Community

Start a new discussion in S32 Design Studio by email or at NXP Community

Following Re: Can you provide me with relevant hardware information about S32R274RRUEVB, such as pin name, pin attribute type, PCB package size data?thank you in these streams: Inbox

This email was sent by NXP Community because you are a registered user.

You may unsubscribe instantly from NXP Community, or adjust email frequency in your email preferences

0 Kudos

1,633 Views
jiri_kral
NXP Employee
NXP Employee

Which type of pins do you mean? On the Motherboard are standard pin headers - detailed description is in second PDF - pages 28-35. On daughter card are high density 240 pin connectors. 

Here is schematics of motherboard itself - https://www.nxp.com/downloads/en/schematics/SCH-27237-MPC57XXMB.pdf 

Here are product details - MPC57XXXMB Product Information|NXP 

The Motherboard PCB size is 260x210 mm (but I can't find this information on our pages - i measured it by myself). 

Jiri

0 Kudos

1,630 Views
shiyu
Contributor I

Hi,jiri

I asked for a change, and the encapsulation of S32R274RRUEVB is 257BGA, 257 pins.I want to know the type of every pin of it, such as: input,output,power.

Can you provide such information?And I want to confirm that its encapsulation is LFBGA257?

Shi

国内首家EPB电子刹车量产企业

The first EPB electronic brake mass production enterprises

浙江力邦合信智能制动系统股份有限公司 石煜 ShiYu

Zhejiang Libang Hexin Intelligent Brake System Co., Ltd.

MOB:15869637318

Postal code:325400

EMAIL: shiyu@cnlbn.com

TEL:0577-63171555

ADD:浙江省平阳万全轻工基地兴隆路111号

No.111, Xinglong Road, Wanquan Light Industrial Zone,

Pingyang County, Zhejiang Province, China.

HTTP:WWW.CNLBN.COM

发件人: jiri.kral@nxp.com

发送时间: 2017-11-28 17:03

收件人: 煜 石

主题: Re: - Re: Can you provide me with relevant hardware information about S32R274RRUEVB, such as pin name, pin attribute type, PCB package size data?thank you

NXP Community

Re: Can you provide me with relevant hardware information about S32R274RRUEVB, such as pin name, pin attribute type, PCB package size data?thank you

reply from Jiri Kral in S32 Design Studio - View the full discussion

Which type of pins do you mean? On the Motherboard are standard pin headers - detailed description is in second PDF - pages 28-35. On daughter card are high density 240 pin connectors.

Here is schematics of motherboard itself - https://www.nxp.com/downloads/en/schematics/SCH-27237-MPC57XXMB.pdf

Here are product details - MPC57XXXMB Product Information|NXP

The Motherboard PCB size is 260x210 mm (but I can't find this information on our pages - i measured it by myself).

Jiri

Reply to this message by replying to this email, or go to the message on NXP Community

Start a new discussion in S32 Design Studio by email or at NXP Community

Following Re: Can you provide me with relevant hardware information about S32R274RRUEVB, such as pin name, pin attribute type, PCB package size data?thank you in these streams: Inbox

This email was sent by NXP Community because you are a registered user.

You may unsubscribe instantly from NXP Community, or adjust email frequency in your email preferences

0 Kudos

1,630 Views
jiri_kral
NXP Employee
NXP Employee

Um - finally - I got it. Here is reference manual for S32R274 - https://www.nxp.com/docs/en/reference-manual/S32R274RM.pdf 

It looks like that you are interested in evaluation board (S32R274RRUEVB) , no in the part itself

Jiri

0 Kudos

1,627 Views
shiyu
Contributor I

Hi

All S32R274 should be 257 pins, right?

What did you mean by " no in the part itself"?Their principle diagram is refer to this -

https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fwww.nxp.com%2Fdownloads%2Fen%2Fschema...

Shi

国内首家EPB电子刹车量产企业

The first EPB electronic brake mass production enterprises

浙江力邦合信智能制动系统股份有限公司 石煜 ShiYu

Zhejiang Libang Hexin Intelligent Brake System Co., Ltd.

MOB:15869637318

Postal code:325400

EMAIL: shiyu@cnlbn.com

TEL:0577-63171555

ADD:浙江省平阳万全轻工基地兴隆路111号

No.111, Xinglong Road, Wanquan Light Industrial Zone,

Pingyang County, Zhejiang Province, China.

HTTP:WWW.CNLBN.COM

发件人: jiri.kral@nxp.com

发送时间: 2017-11-28 19:58

收件人: 煜 石

主题: Re: - Re: Can you provide me with relevant hardware information about S32R274RRUEVB, such as pin name, pin attribute type, PCB package size data?thank you

NXP Community

Re: Can you provide me with relevant hardware information about S32R274RRUEVB, such as pin name, pin attribute type, PCB package size data?thank you

reply from Jiri Kral in S32 Design Studio - View the full discussion

Um - finally - I got it. Here is reference manual for S32R274 - https://www.nxp.com/docs/en/reference-manual/S32R274RM.pdf

It looks like that you are interested in evaluation board (S32R274RRUEVB) , no in the part itself

Jiri

Reply to this message by replying to this email, or go to the message on NXP Community

Start a new discussion in S32 Design Studio by email or at NXP Community

Following Re: Can you provide me with relevant hardware information about S32R274RRUEVB, such as pin name, pin attribute type, PCB package size data?thank you in these streams: Inbox

This email was sent by NXP Community because you are a registered user.

You may unsubscribe instantly from NXP Community, or adjust email frequency in your email preferences

0 Kudos

1,627 Views
jiri_kral
NXP Employee
NXP Employee

Hi Shi, 

yes - S32R274 (the MCU) is in the 257-ball MAPBGA, 0.8 mm ball pitch, 14 mm x 14 mm outline package. 

We are also providing evaluation board - the S32R274RRUEVB. This evaluation board can be attached into MPC57XX Motherboard. Motherboard provides access into all pins and peripherals in user friendly way (pin headers/connectors). It is not obvious from your question in which part you are interested in. 

Jiri

0 Kudos