GHS plug-in Can not successfully installed in S32DS for Power Architecture version 2017.R1

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

GHS plug-in Can not successfully installed in S32DS for Power Architecture version 2017.R1

1,492件の閲覧回数
yyang
Contributor II

Dear Engineer:

I update  S32 Design Studio for Power Architecture from version v1.2 to version 2017.R1.I found a issue ,when I integrated the GHS compiler toolchain in S32DS there was an error .

1.bmp

Details:

Cannot complete the install because one or more required items could not be found.
Software being installed: Green Hills MULTI for Eclipse (PowerPC) 2.1.9 (ghs.multi.ppc.feature.group 2.1.9)

Missing requirement: MULTI Plug-in 2.1.9 (ghs.launch.multi 2.1.9) requires 'bundle org.eclipse.cdt.debug.mi.core 0.0.0' but it could not be found

Cannot satisfy dependency:
 From: Green Hills MULTI for Eclipse (PowerPC) 2.1.9 (ghs.multi.ppc.feature.group 2.1.9)
 To: ghs.launch.multi [2.1.9]

I uninstalled the S32DS and GHS to reinstall,the problem will still appear.

I do not have this problem When I use S32DS for Power Architecture version v1.2.

Best Regards!

0 件の賞賛
返信
1 返信

1,175件の閲覧回数
stanish
NXP Employee
NXP Employee
0 件の賞賛
返信