Add FreeRTOS on S32 DS 3.4 project for a S32K3-T-BOX

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Add FreeRTOS on S32 DS 3.4 project for a S32K3-T-BOX

跳至解决方案
952 次查看
Rab06
Contributor I

Hello,

I have an actual project running on S32 Design Studio for S32 Platform V3.4 with RTD 2.0.1.

I want to update it to use FreeRTOS for the moment and migrate it to SafeRTOS later.


I don't find any packages for FreeRTOS on S32K3xx, there is any package library to add with this software and easy configuration tools or i have to add manually the FreeRTOS ?

Is it better to work on S32 DS for ARM to work with FreeRTOS on this S32K3-T-BOX board ?

Thank you.

0 项奖励
回复
1 解答
942 次查看
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @Rab06 

FreeRTOS packages can be found in S32K3 Reference Software package:

https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=SW32K3-REFSW-D

lukaszadrapa_0-1696942207093.png

 lukaszadrapa_1-1696942218319.png

S32DS for ARM does not support S32K3 devices, use S32DS for S32 Platform instead.

Regards,

Lukas

 

在原帖中查看解决方案

0 项奖励
回复
2 回复数
943 次查看
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @Rab06 

FreeRTOS packages can be found in S32K3 Reference Software package:

https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=SW32K3-REFSW-D

lukaszadrapa_0-1696942207093.png

 lukaszadrapa_1-1696942218319.png

S32DS for ARM does not support S32K3 devices, use S32DS for S32 Platform instead.

Regards,

Lukas

 

0 项奖励
回复
906 次查看
Rab06
Contributor I
Thank you.

I found this link on the same way with installation details : https://community.nxp.com/t5/S32K/S32K314-try-to-build-a-project-with-freertos/m-p/1516169#M17482

BR,
Rabah
0 项奖励
回复