This document contains the instructions how to download separate elf/srec/hex file to the microcontroller using S32 Design Studio and USB PE Micro Universal Multilink/OpenSDA debug probes. This could be used in case you get an executable/binary image file only without any project or source code.
There are basically three ways:
Click on "Flash" button to proceed to programming. As soon as the device is programmed it's disconnected.
2. Executable file importer. Go to menu File -> Import -> Select "Executable File Importer" this starts the wizard. This is for programming and debugging an executable elf object file only.
3. reuse an existing project debug configuration or create a new dummy project for loading .elf/srec/hex
Hi b55689,
very straight forward explanation !
One question. I wonder if downloading by using Multilink is 'much' faster than via embedded chipsets (FTDI, OpenSDA, etc.)? I work from a Win10 VM, so it can take in the seconds (10+) to download.
Thanks,
Ludwig
Dear Support Team
Explanation is very simple, but it is for S23DS Power 1.2+, unfortunatelly I cant find that version available for download.
There is only S32DS Power 1.1 which hasn't got that functionality.
When do you have plan to publish new version of S32DS for Power Architecture?
best regards
Marek
Hello Marek,
S32 Design Studio for power version 1.2 should be released at the end of May.
Regards,
Martin
Hi, Martin:
Very clear explaination!
If I only have .hex file of SPC5744P project, can I use the 2nd method or the 3rd method you mentioned? or I have to wait for "S32DS for PA1.2" available for download?
Best Regards
William Wang
Hello William,
to be honest, I do not know. I have never tried to work with hex file (I tested srecord and elf only). But if you contact Stanislav Sliva, he will provide you more accurate information regarding this "problem".
Regards,
Martin
Hello Jed,
release date is postponed to 16 June, because of fixing critical compiler issue.
Regards,
Martin
Dear Support Team:
The MPC5748G has three cores。what core is correct when I just have only one elf file?(For about the third way)
I tried new a "hellow" project from example in S32 Design Studio for Power Architecture Version 2.1 and chose core0 to debug .But it failed.