S32 Design Studio (S32DS) for ARM supports IAR Eclipse plug-in that enables users to build and debug a S32DS project with IAR toolchain for ARM.
This document describes how to install this plugin and how to enable IAR in the new project wizard.
Current version of S32DS for ARM 2018.R1 supports IAR compilers v7.x and v8.x.
After the IAR eclipse plugin installation is finished you should be able to create, build and debug a new S32DS project (including SDKs) using IAR compiler/debugger interface directly under S32DS Eclipse environment.
First of all make sure you have IAR Embedded Workbench installed with a valid license from IAR. Now let's proceed to eclipse plug-in installation.
Enjoy building and debugging with IAR Eclipse plug-in in S32DS!
hello. Stanislav Sliva
I want to use IAR compiler. so I install IAR Plugin manager like you.
But I encountered the following problem during installation.
\
After installation, I did check 'window->preferences'. but there is no 'IAR Embedded Workbench'
As shown in the picture below, I can not proceed with the installation any more.
Please check this problem.
Best regards
MinYeop