s12zvml31 Motor driver transplant

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

s12zvml31 Motor driver transplant

913件の閲覧回数
mine233
Contributor I

I want to transplant the motor driver program based on s12zvml128 to s12zvml31. The modified program can be burned to the development board of s12zvml31, but the motor cannot run, and the program transplanted to s12zvml31 cannot enter the ADC interrupt, so the foc algorithm cannot be performed. Do the ADC, timer, and interrupt of s12zvml128 and s12zvml31 need to be configured accordingly?

0 件の賞賛
返信
2 返答(返信)

901件の閲覧回数
lama
NXP TechSupport
NXP TechSupport

Hi,

I hope this AN will help you...

https://www.nxp.com/docs/en/application-note/AN5330.pdf

 

Best regards,

Ladislav

0 件の賞賛
返信

888件の閲覧回数
mine233
Contributor I

According to the modification of this document, the program can now run normally on s12zvml31, but the oil pump motor still cannot work normally. Do you need to send external signals through freemaster software to drive the motor?

0 件の賞賛
返信