s12zvml31 Motor driver transplant

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

s12zvml31 Motor driver transplant

903 Views
mine233
Contributor I

I want to transplant the motor driver program based on s12zvml128 to s12zvml31. The modified program can be burned to the development board of s12zvml31, but the motor cannot run, and the program transplanted to s12zvml31 cannot enter the ADC interrupt, so the foc algorithm cannot be performed. Do the ADC, timer, and interrupt of s12zvml128 and s12zvml31 need to be configured accordingly?

0 Kudos
Reply
2 Replies

891 Views
lama
NXP TechSupport
NXP TechSupport

Hi,

I hope this AN will help you...

https://www.nxp.com/docs/en/application-note/AN5330.pdf

 

Best regards,

Ladislav

0 Kudos
Reply

878 Views
mine233
Contributor I

According to the modification of this document, the program can now run normally on s12zvml31, but the oil pump motor still cannot work normally. Do you need to send external signals through freemaster software to drive the motor?

0 Kudos
Reply