Hi
the pin is use to select oscillator configuration during reset.
(You do not mention the MCU number.)
For example, in the case of S12XEP100 (Table 1-10. Signal Properties Summary) the pin is pulled up during reset. In your configuration it will read log. level = 0 and the MCU sets oscilator configuration corresponding to this level.
After reset the pin is set as Hi-Z input pin because DDRE.7 = 0 (reset status)....chapter 2.3.12
If you set it as output port (DDRE.7 = 1) and you use it as ECLKX2output or you prite to the pin log.1 then it cause shortcut.
If it is grounded in your design you have to ensure the pin will newer be set as output pin with log.1 written to it.
So finally; the configuration is possible but unsafe.
Best regards,
Ladislav
Hi
the pin is use to select oscillator configuration during reset.
(You do not mention the MCU number.)
For example, in the case of S12XEP100 (Table 1-10. Signal Properties Summary) the pin is pulled up during reset. In your configuration it will read log. level = 0 and the MCU sets oscilator configuration corresponding to this level.
After reset the pin is set as Hi-Z input pin because DDRE.7 = 0 (reset status)....chapter 2.3.12
If you set it as output port (DDRE.7 = 1) and you use it as ECLKX2output or you prite to the pin log.1 then it cause shortcut.
If it is grounded in your design you have to ensure the pin will newer be set as output pin with log.1 written to it.
So finally; the configuration is possible but unsafe.
Best regards,
Ladislav