/XCLKS Is direct grounding OK?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

/XCLKS Is direct grounding OK?

ソリューションへジャンプ
1,875件の閲覧回数
nxpxhy13
Contributor I

My CPU is mc9s12xe series,The external crystal oscillator is used。

0 件の賞賛
返信
1 解決策
1,865件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hello,

To configure the the oscillator for Full Swing Pierce or for an external clock source, the pin must read LOW during rising edge of the reset pin signal.

It can be either driven or pulled externally. 

Please note that the the pin has an internal weak pullup enabled by default out of reset.

danielmartynek_0-1602665365520.png

So, if an external pull-down is used, it must be stronger than that to ensure the logic value and compensate for noise.

If the pin is connected to the ground directly, make sure the SW does not reconfigure the pin to GPIO Output and does not drive it HIGH.

 

Reference schematics for S12(X) devices:

https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Reference-schematics-for-S12-X-devices/ta-p...

danielmartynek_1-1602665602931.png

 

Regards,

Daniel

 

 

 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,866件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hello,

To configure the the oscillator for Full Swing Pierce or for an external clock source, the pin must read LOW during rising edge of the reset pin signal.

It can be either driven or pulled externally. 

Please note that the the pin has an internal weak pullup enabled by default out of reset.

danielmartynek_0-1602665365520.png

So, if an external pull-down is used, it must be stronger than that to ensure the logic value and compensate for noise.

If the pin is connected to the ground directly, make sure the SW does not reconfigure the pin to GPIO Output and does not drive it HIGH.

 

Reference schematics for S12(X) devices:

https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Reference-schematics-for-S12-X-devices/ta-p...

danielmartynek_1-1602665602931.png

 

Regards,

Daniel

 

 

 

0 件の賞賛
返信