What's the difference between S912ZVCA96AMLF and S912ZVCA96F0MLF?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

What's the difference between S912ZVCA96AMLF and S912ZVCA96F0MLF?

跳至解决方案
2,515 次查看
Edgar_Jiang
Contributor II

hi

Could you help me to find the difference between S912ZVCA96AMLF and S912ZVCA96F0MLF?My client want to order S912ZVCA96F0MLF, but we could only find S912ZVCA96AML.If they are same in function?

0 项奖励
回复
1 解答
2,507 次查看
lama
NXP TechSupport
NXP TechSupport

Hi,

S912ZVCA96F0MLF has a mask set 0N23N. The S912ZVCA96AMLF has the same mask set .

The change (from F0 to A) was done because it is possible the device can be manufactured in different factory. In the past we used different mask set numbers for the same mask if the device was manufactured in different factory. There was a PCN published in past. The PCN unifies the same mask set with different codes to a common code A,B,C,… when the reason of different mask set number is the only manufacturing  site.

So, both devices are absolutely the same.

Best regards,

Ladislav

在原帖中查看解决方案

7 回复数
2,339 次查看
lama
NXP TechSupport
NXP TechSupport

Hi,

F0 is manufactured in ATMC.

However, A does not say about manufacturing site. It can be ATMC as well as TSMC. It is not recognizable.

Best regards,

Ladislav

1,154 次查看
caesar_song
Contributor III
 
0 项奖励
回复
2,335 次查看
Edgar_Jiang
Contributor II

OK,thanks for your reply!

0 项奖励
回复
2,508 次查看
lama
NXP TechSupport
NXP TechSupport

Hi,

S912ZVCA96F0MLF has a mask set 0N23N. The S912ZVCA96AMLF has the same mask set .

The change (from F0 to A) was done because it is possible the device can be manufactured in different factory. In the past we used different mask set numbers for the same mask if the device was manufactured in different factory. There was a PCN published in past. The PCN unifies the same mask set with different codes to a common code A,B,C,… when the reason of different mask set number is the only manufacturing  site.

So, both devices are absolutely the same.

Best regards,

Ladislav

1,144 次查看
caesar_song
Contributor III

Hi Could you help to provide the ducument of  F0 and A for 

S9S12ZVLS3F0VFMR and S9S12ZVLS3AVFMR   ,thanks

0 项奖励
回复
1,970 次查看
Edgar_Jiang
Contributor II
How about SPC5643LK0MLQ1 and SPC5643LAMLQ1? If them also meet this condition?
0 项奖励
回复
2,347 次查看
Edgar_Jiang
Contributor II
Dear Ladislav 
 
I need to know if the wafers of F0 and A are all OEM by TSMC? Could you help me to confirm this?
 
Best regards,
 
Edgar
0 项奖励
回复