What's the difference between S912ZVCA96AMLF and S912ZVCA96F0MLF?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What's the difference between S912ZVCA96AMLF and S912ZVCA96F0MLF?

ソリューションへジャンプ
2,348件の閲覧回数
Edgar_Jiang
Contributor II

hi

Could you help me to find the difference between S912ZVCA96AMLF and S912ZVCA96F0MLF?My client want to order S912ZVCA96F0MLF, but we could only find S912ZVCA96AML.If they are same in function?

0 件の賞賛
返信
1 解決策
2,340件の閲覧回数
lama
NXP TechSupport
NXP TechSupport

Hi,

S912ZVCA96F0MLF has a mask set 0N23N. The S912ZVCA96AMLF has the same mask set .

The change (from F0 to A) was done because it is possible the device can be manufactured in different factory. In the past we used different mask set numbers for the same mask if the device was manufactured in different factory. There was a PCN published in past. The PCN unifies the same mask set with different codes to a common code A,B,C,… when the reason of different mask set number is the only manufacturing  site.

So, both devices are absolutely the same.

Best regards,

Ladislav

元の投稿で解決策を見る

7 返答(返信)
2,172件の閲覧回数
lama
NXP TechSupport
NXP TechSupport

Hi,

F0 is manufactured in ATMC.

However, A does not say about manufacturing site. It can be ATMC as well as TSMC. It is not recognizable.

Best regards,

Ladislav

987件の閲覧回数
caesar_song
Contributor III
 
0 件の賞賛
返信
2,168件の閲覧回数
Edgar_Jiang
Contributor II

OK,thanks for your reply!

0 件の賞賛
返信
2,341件の閲覧回数
lama
NXP TechSupport
NXP TechSupport

Hi,

S912ZVCA96F0MLF has a mask set 0N23N. The S912ZVCA96AMLF has the same mask set .

The change (from F0 to A) was done because it is possible the device can be manufactured in different factory. In the past we used different mask set numbers for the same mask if the device was manufactured in different factory. There was a PCN published in past. The PCN unifies the same mask set with different codes to a common code A,B,C,… when the reason of different mask set number is the only manufacturing  site.

So, both devices are absolutely the same.

Best regards,

Ladislav

977件の閲覧回数
caesar_song
Contributor III

Hi Could you help to provide the ducument of  F0 and A for 

S9S12ZVLS3F0VFMR and S9S12ZVLS3AVFMR   ,thanks

0 件の賞賛
返信
1,803件の閲覧回数
Edgar_Jiang
Contributor II
How about SPC5643LK0MLQ1 and SPC5643LAMLQ1? If them also meet this condition?
0 件の賞賛
返信
2,180件の閲覧回数
Edgar_Jiang
Contributor II
Dear Ladislav 
 
I need to know if the wafers of F0 and A are all OEM by TSMC? Could you help me to confirm this?
 
Best regards,
 
Edgar
0 件の賞賛
返信