Hello, I have a universal BDM12 from technological arts.I have been unable to download S records to the 9S12NE64 CPU flash using the BDM. I have erased the flash using the fbulk command. I have used the ;np and ;b options too. It is giving me the following error: Bad Hex Data Here is a snapshot of my s-records: All S1 records are of equal length.
S00F00007374362D3531312E696D67D4 S123400006404D85505041474500004CC8003086494E4954524D40034CC800108453594E95 S123402052400F4CC80034855245464456401C4CC8003586435247464C4740274CC8003705 S123404086434C4B53454C40334CC8003986115A10863CF6F82B2602863D5A30D726030601 S12340608004064C4A85504F52544140404CC8000085504F52544240654CC80001844444AB ---------------------------------------- S12380004CC8002E85414354535A7FF84CC80020864C475442535A80044CC80044864C4714 S123802043484B3180104CC80045854C47535A31801D4CC8004685544147535A802A4CC893 S12380400020875441475442535A80364CC800E18845455F534348454480424CC800008974 ----------------------------------- S123C0000010B4265582BB0CB560B2A2C0714D5A000CBDACBB25B560B2A2BF294D5A002ED8 S123C020BD1B4D650028BC3E4D650018BBDB4D520010B4265582BB0CB560B2A2C0714D5A88 S123C040000CBC85BB0CB560B2A2BF70BC664D65000CB617C133B560B2A2BA0DB560B2A2F6 ------------------------------------ S123FEE000000000000000000000000000000000000000000000000000000000BC82DD8C57 S123FF0000000000000000000000FFFFFFFFFFFE105354362D3531312E30303220202020F3 S123FF20000035000200000000000000000000000000000000000000000000000000000086 S123FF4000000000000000000000000000000000000000000000000000000000000000009D S123FF6000000000000000000000000000000000000000000000000000000000000000007D S123FF8000000000000000000000000010841087108A108D1090109310961099109C109F0E S123FFA010A210A510A810AB10AE10B110B410B710BA10BD10C010C310C610C910CC10CFB5 S123FFC010D210D510D810DB10DE10E110E410E710EA10ED10F010F310F610F910FC10FF95 S123FFE0110211051108110B110E111111141117111A111D112011234C3D4C454C48400065 S90380007C Any hints on the problem will be much appreciated. Thanks, Lav