Unable to download S19 file to 9S12NE64 using D-BUG12

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Unable to download S19 file to 9S12NE64 using D-BUG12

ソリューションへジャンプ
2,158件の閲覧回数
LT
Contributor I
Hello,
         I have a universal BDM12 from technological arts.I have been unable to download S records to the
9S12NE64 CPU flash using the BDM. I have erased the flash using the fbulk command. I have used the
;np and ;b options too.
It is giving me the following error: Bad Hex Data
Here is a snapshot of my s-records:
All S1 records are of equal length.

S00F00007374362D3531312E696D67D4
S123400006404D85505041474500004CC8003086494E4954524D40034CC800108453594E95
S123402052400F4CC80034855245464456401C4CC8003586435247464C4740274CC8003705
S123404086434C4B53454C40334CC8003986115A10863CF6F82B2602863D5A30D726030601
S12340608004064C4A85504F52544140404CC8000085504F52544240654CC80001844444AB
 ----------------------------------------
S12380004CC8002E85414354535A7FF84CC80020864C475442535A80044CC80044864C4714
S123802043484B3180104CC80045854C47535A31801D4CC8004685544147535A802A4CC893
S12380400020875441475442535A80364CC800E18845455F534348454480424CC800008974
 -----------------------------------
S123C0000010B4265582BB0CB560B2A2C0714D5A000CBDACBB25B560B2A2BF294D5A002ED8
S123C020BD1B4D650028BC3E4D650018BBDB4D520010B4265582BB0CB560B2A2C0714D5A88
S123C040000CBC85BB0CB560B2A2BF70BC664D65000CB617C133B560B2A2BA0DB560B2A2F6
------------------------------------
S123FEE000000000000000000000000000000000000000000000000000000000BC82DD8C57
S123FF0000000000000000000000FFFFFFFFFFFE105354362D3531312E30303220202020F3
S123FF20000035000200000000000000000000000000000000000000000000000000000086
S123FF4000000000000000000000000000000000000000000000000000000000000000009D
S123FF6000000000000000000000000000000000000000000000000000000000000000007D
S123FF8000000000000000000000000010841087108A108D1090109310961099109C109F0E
S123FFA010A210A510A810AB10AE10B110B410B710BA10BD10C010C310C610C910CC10CFB5
S123FFC010D210D510D810DB10DE10E110E410E710EA10ED10F010F310F610F910FC10FF95
S123FFE0110211051108110B110E111111141117111A111D112011234C3D4C454C48400065
S90380007C
Any hints on the problem will be much appreciated.
Thanks,
Lav
ラベル(1)
0 件の賞賛
返信
1 解決策
1,379件の閲覧回数
wolfgang_b
Contributor II

I fixed my "Bad Hex Data" error by setting my flowcontrol to Xon/Xoff.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,380件の閲覧回数
wolfgang_b
Contributor II

I fixed my "Bad Hex Data" error by setting my flowcontrol to Xon/Xoff.

0 件の賞賛
返信
1,379件の閲覧回数
blood
Contributor III
What are those dashed lines there for? You're not trying to download them as part of the s19 are you?
0 件の賞賛
返信