S912ZVML Hall Sensored BLDC motor

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S912ZVML Hall Sensored BLDC motor

711 Views
pratibhasurabhi
Contributor V

Hi,

 

I am working on MTRCKTSBNZVM128 eval kit .

I am running Hall sensored motor algorithm firmware.

The sample code is provided by NXP itself.

 

Query is only 

Motor RPM calculation I found is to be incorrect.

Observing the HallPeriod array and Hall patterns,only 3 Hall pattern sequences are observed (4,5,6).

So the commutation is found to be not 120 commutation.

 

Please guide as to how to rectify the commutation issue,such that all hall patterns are observed.

Tags (2)
2 Replies

450 Views
pratibhasurabhi
Contributor V

Also I have another query.

I am using the ZVML64 where PT3-1 are used for Hall Sensor signals and IOCO_0 is used for capturing PWM input

Is it possible to use them simultaneously?

0 Kudos

450 Views
pratibhasurabhi
Contributor V

It was an hardware issue.

Rectified it.

Also would like to know MOTOR_STALL_1MS_COUNT,HallPeriodMax(10900) was defined?

0 Kudos