Reset pin on MC9S12XEQ pulls down for unknown reason

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Reset pin on MC9S12XEQ pulls down for unknown reason

跳至解决方案
408 次查看
programmer
Contributor I

Hello,

 

I've started writing code for the MC9S12XEQ.

The code resets the COP watchdog timer by writing 0x55 and 0xAA, but for unknown reason, the RESET pin pulls down for 1.5 ms every 50 milliseconds.

 

This is also happens whenever the debugger stops the MCU (which is logical, but it also happens when the debugger is not connected).

 

How can I keep the RESET pin always up?

 

Thank you.

标签 (1)
0 项奖励
1 解答
301 次查看
kef
Specialist I

S12XE pulls RESET pin low when internal reset occurs. It could be illegal address reset, COP or clock monitor reset.

在原帖中查看解决方案

0 项奖励
1 回复
302 次查看
kef
Specialist I

S12XE pulls RESET pin low when internal reset occurs. It could be illegal address reset, COP or clock monitor reset.

0 项奖励