Hi Kiran,
I see 16byte shift in your table.
PortAD interrupt vector should be on address = Vector base + 0xF4.
The same way are shifted also other interrupt vectors.
I started my vector table from address 0xFFF610 and my table has 123 vectors.
When you start table without that offset (0x10), you table should contain 127 vectors (the last/first vector is reset vector).
Note: 128 x 4B vector size = 512B
I hope it helps you.
Have a great day,
Radek
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
I prepared for you very simple example project with relocated interrupt vector table into RAM/Flash.
See attachment.
I hope it helps you.
Have a great day,
Radek
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Radek
Thanks for the example. But i have one issue, whichever interrupt is configured each time on Unimplemented section is executed. I am pasting the code (Not able to attach the project) please check and correct me where i am wrong.
/*****************************Mani.c**********************************************/
#include <hidef.h> /* for EnableInterrupts macro */
#include "derivative.h" /* include peripheral declarations */
//#include "VectorTable.h"
void BSP_PIM_HLUWAKE_Interrupt_Enable(void);
unsigned int i;
void main(void)
{
//IVBR=(INT_VECTOR_TABLE_ADDR_IN_FLASH & 0xFFFFFE)>>8;
IVBR = 0xFEC4;
DDRP_DDRP0 = 1;
DDRP_DDRP4 = 1;
DDRP_DDRP5 = 1;
PTP_PTP0 = 1;
PTP_PTP4 = 1;
PTP_PTP5 = 1;
BSP_PIM_HLUWAKE_Interrupt_Enable();
EnableInterrupts;
/* include your code here */
for(;;)
{
PTP_PTP0 = ~PTP_PTP0;
for(i = 0; i< 20000; i++);
}
}
void BSP_PIM_HLUWAKE_Interrupt_Enable(void)
{
/*configure port AD for KWU feature*/
DDRAD_DDRADL3 = 0; /* Configure PAD3 as input */
DIENADL_DIENADL3 = 1; /* Pin is configured as digital input */
PERAD_PERADL3 = 0; /* Enable Pull Device on PAD3 */
PPSAD_PPSADL3 = 1; /* Configure interrupt for Rising Edge */
PIEAD_PIEADL3 = 1; /* Enable Interrupt on PAD3 (KWAD3) */
}
/***************************** End Mani.c**********************************************/
/******************************VectorTable.c*****************************************/
/*
* VectorTable.c
*
* Created on: Jun 29, 2016
* Author: kiran.bhat
*/
#include "VectorTable.h"
//==============================================================================
// Unimplemented_ISR
//==============================================================================
interrupt void Unimplemented_ISR(void)
{
//PTP_PTP5 = ~PTP_PTP5;
//PIFADL_PIFADL3 = 1;
asm NOP; //place breakpoint here
}
interrupt void WakeUpISR(void)
{
PIFADL_PIFADL3 = 1;
PTP_PTP4 = ~PTP_PTP4;
}
/***************************** End VectorTable.c**********************************************/
/******************************VectorTable.h*****************************************/
/******************************End VectorTable.h*****************************************/
Regards
Kiran
/******************************VectorTable.h*****************************************/
/*
* VectorTable.h
*
* Created on: Jun 29, 2016
* Author: kiran.bhat
*/
#ifndef VECTORTABLE_H_
#define VECTORTABLE_H_
#include "derivative.h" /* include peripheral declarations */
#define INT_VECTOR_TABLE_ADDR_IN_FLASH 0xFEC400
#define INT_VECTOR_TABLE_SIZE 123
//Please see prm linker file where we removed area with vector table from linker usage.
/* ISR prototype */
interrupt void WakeUpISR(void);
interrupt void Unimplemented_ISR(void);
//vector table defined in Flash
typedef void (*const tIsrFunc)(void);
/* Pack 3 byte pointers as 4 byte Interrupt Vector Table entries */
typedef struct
{
byte padding;
tIsrFunc address;
} InterruptTableEntry;
#define _VECTOR(v) {0xFFU, &v}
//Please replace aprropriate Unimplemented_ISR by implemented interrupt routine
//see Table 1-13. Interrupt Vector Locations in RM for more details
const InterruptTableEntry _InterruptVectorTable[INT_VECTOR_TABLE_SIZE] @INT_VECTOR_TABLE_ADDR_IN_FLASH = { /* Interrupt vector table */
_VECTOR(Unimplemented_ISR),//0x00 VReserved123
_VECTOR(Unimplemented_ISR),//0x04 VReserved122
_VECTOR(Unimplemented_ISR),//0x08 VReserved121
_VECTOR(Unimplemented_ISR),//0x0C VReserved120
_VECTOR(Unimplemented_ISR),//0x10 VReserved119
_VECTOR(Unimplemented_ISR),//0x14 VReserved118
_VECTOR(Unimplemented_ISR),//0x18 VReserved117
_VECTOR(Unimplemented_ISR),//0x1C VReserved116
_VECTOR(Unimplemented_ISR),//0x20 VReserved115
_VECTOR(Unimplemented_ISR),//0x24 VReserved114
_VECTOR(Unimplemented_ISR),//0x28 VReserved113
_VECTOR(Unimplemented_ISR),//0x2C VReserved112
_VECTOR(Unimplemented_ISR),//0x30 VReserved111
_VECTOR(Unimplemented_ISR),//0x34 VReserved110
_VECTOR(Unimplemented_ISR),//0x38 VReserved109
_VECTOR(Unimplemented_ISR),//0x3C VReserved108
_VECTOR(Unimplemented_ISR),//0x40 VReserved107
_VECTOR(Unimplemented_ISR),//0x44 VReserved106
_VECTOR(Unimplemented_ISR),//0x48 VReserved105
_VECTOR(Unimplemented_ISR),//0x4C Vsenttx
_VECTOR(Unimplemented_ISR),//0x50 Viic
_VECTOR(Unimplemented_ISR),//0x54 VReserved102
_VECTOR(Unimplemented_ISR),//0x58 VReserved101
_VECTOR(Unimplemented_ISR),//0x5C VReserved100
_VECTOR(Unimplemented_ISR),//0x60 VReserved99
_VECTOR(Unimplemented_ISR),//0x64 VReserved98
_VECTOR(Unimplemented_ISR),//0x68 VReserved97
_VECTOR(Unimplemented_ISR),//0x6C VReserved96
_VECTOR(Unimplemented_ISR),//0x70 VReserved95
_VECTOR(Unimplemented_ISR),//0x74 VReserved94
_VECTOR(Unimplemented_ISR),//0x78 VReserved93
_VECTOR(Unimplemented_ISR),//0x7C Vtim1ovf
_VECTOR(Unimplemented_ISR),//0x80 VReserved91
_VECTOR(Unimplemented_ISR),//0x84 VReserved90
_VECTOR(Unimplemented_ISR),//0x88 VReserved89
_VECTOR(Unimplemented_ISR),//0x8C VReserved88
_VECTOR(Unimplemented_ISR),//0x90 Vtim1ch3
_VECTOR(Unimplemented_ISR),//0x94 Vtim1ch2
_VECTOR(Unimplemented_ISR),//0x98 Vtim1ch1
_VECTOR(Unimplemented_ISR),//0x9C Vtim1ch0
_VECTOR(Unimplemented_ISR),//0xA0 VReserved83
_VECTOR(Unimplemented_ISR),//0xA4 VReserved82
_VECTOR(Unimplemented_ISR),//0xA8 VReserved81
_VECTOR(Unimplemented_ISR),//0xAC VReserved80
_VECTOR(Unimplemented_ISR),//0xB0 Vportl
_VECTOR(Unimplemented_ISR),//0xB4 VReserved78
_VECTOR(Unimplemented_ISR),//0xB8 VReserved77
_VECTOR(Unimplemented_ISR),//0xBC VReserved76
_VECTOR(Unimplemented_ISR),//0xC0 VReserved75
_VECTOR(Unimplemented_ISR),//0xC4 VReserved74
_VECTOR(Unimplemented_ISR),//0xC8 VReserved73
_VECTOR(Unimplemented_ISR),//0xCC VReserved72
_VECTOR(Unimplemented_ISR),//0xD0 VReserved71
_VECTOR(Unimplemented_ISR),//0xD4 VReserved70
_VECTOR(Unimplemented_ISR),//0xD8 VReserved69
_VECTOR(Unimplemented_ISR),//0xDC VReserved68
_VECTOR(Unimplemented_ISR),//0xE0 VReserved67
_VECTOR(WakeUpISR), //0xE4 Vportad
_VECTOR(Unimplemented_ISR),//0xE8 VReserved65
_VECTOR(Unimplemented_ISR),//0xEC Vhti
_VECTOR(Unimplemented_ISR),//0xF0 Vapi
_VECTOR(Unimplemented_ISR),//0xF4 Vlvi
_VECTOR(Unimplemented_ISR),//0xF8 Vevddx
_VECTOR(Unimplemented_ISR),//0xFC Vportp
_VECTOR(Unimplemented_ISR),//0x100 VReserved59
_VECTOR(Unimplemented_ISR),//0x104 VReserved58
_VECTOR(Unimplemented_ISR),//0x108 VReserved57
_VECTOR(Unimplemented_ISR),//0x10C VReserved56
_VECTOR(Unimplemented_ISR),//0x110 VReserved55
_VECTOR(Unimplemented_ISR),//0x114 Vports
_VECTOR(Unimplemented_ISR),//0x118 Vcanphy0
_VECTOR(Unimplemented_ISR),//0x11C VReserved52
_VECTOR(Unimplemented_ISR),//0x120 VReserved51
_VECTOR(Unimplemented_ISR),//0x124 VReserved50
_VECTOR(Unimplemented_ISR),//0x128 VReserved49
_VECTOR(Unimplemented_ISR),//0x12C VReserved48
_VECTOR(Unimplemented_ISR),//0x130 Vbats
_VECTOR(Unimplemented_ISR),//0x134 VReserved46
_VECTOR(Unimplemented_ISR),//0x138 VReserved45
_VECTOR(Unimplemented_ISR),//0x13C VReserved44
_VECTOR(Unimplemented_ISR),//0x140 Vcan0tx
_VECTOR(Unimplemented_ISR),//0x144 Vcan0rx
_VECTOR(Unimplemented_ISR),//0x148 Vcan0err
_VECTOR(Unimplemented_ISR),//0x14C Vcan0wkup
_VECTOR(Unimplemented_ISR),//0x150 Vflash
_VECTOR(Unimplemented_ISR),//0x154 Vflasherr
_VECTOR(Unimplemented_ISR),//0x158 VReserved37
_VECTOR(Unimplemented_ISR),//0x15C Vspi1
_VECTOR(Unimplemented_ISR),//0x160 VRAM_err
_VECTOR(Unimplemented_ISR),//0x164 Vacmp1
_VECTOR(Unimplemented_ISR),//0x168 Vacmp0
_VECTOR(Unimplemented_ISR),//0x16C Vcpmuplllck
_VECTOR(Unimplemented_ISR),//0x170 Vcpmuosc
_VECTOR(Unimplemented_ISR),//0x174 Vadc0conv_compl
_VECTOR(Unimplemented_ISR),//0x178 Vadc0conv_seq_abrt
_VECTOR(Unimplemented_ISR),//0x17C Vadc0err
_VECTOR(Unimplemented_ISR),//0x180 VReserved27
_VECTOR(Unimplemented_ISR),//0x184 VReserved26
_VECTOR(Unimplemented_ISR),//0x188 Vsci1
_VECTOR(Unimplemented_ISR),//0x18C Vsci0
_VECTOR(Unimplemented_ISR),//0x190 Vspi0
_VECTOR(Unimplemented_ISR),//0x194 Vtim0paie
_VECTOR(Unimplemented_ISR),//0x198 Vtim0paaovf
_VECTOR(Unimplemented_ISR),//0x19C Vtim0ovf
_VECTOR(Unimplemented_ISR),//0x1A0 Vtim0ch7
_VECTOR(Unimplemented_ISR),//0x1A4 Vtim0ch6
_VECTOR(Unimplemented_ISR),//0x1A8 Vtim0ch5
_VECTOR(Unimplemented_ISR),//0x1AC Vtim0ch4
_VECTOR(Unimplemented_ISR),//0x1B0 Vtim0ch3
_VECTOR(Unimplemented_ISR),//0x1B4 Vtim0ch2
_VECTOR(Unimplemented_ISR),//0x1B8 Vtim0ch1
_VECTOR(Unimplemented_ISR),//0x1BC Vtim0ch0
_VECTOR(Unimplemented_ISR),//0x1C0 Vrti
_VECTOR(Unimplemented_ISR),//0x1C4 Virq
_VECTOR(Unimplemented_ISR),//0x1C8 Vxirq
_VECTOR(Unimplemented_ISR),//0x1CC Vsi
_VECTOR(Unimplemented_ISR),//0x1D0 VReserved7
_VECTOR(Unimplemented_ISR),//0x1D4 VReserved6
_VECTOR(Unimplemented_ISR),//0x1D8 Vme
_VECTOR(Unimplemented_ISR),//0x1DC Vsys
_VECTOR(Unimplemented_ISR),//0x1E0 Vswi
_VECTOR(Unimplemented_ISR),//0x1E4 Vtrap
_VECTOR(Unimplemented_ISR),//0x1E8 Vspare
};
#endif /* VECTORTABLE_H_ */
/******************************End VectorTable.h*****************************************/
Hi Kiran,
I see 16byte shift in your table.
PortAD interrupt vector should be on address = Vector base + 0xF4.
The same way are shifted also other interrupt vectors.
I started my vector table from address 0xFFF610 and my table has 123 vectors.
When you start table without that offset (0x10), you table should contain 127 vectors (the last/first vector is reset vector).
Note: 128 x 4B vector size = 512B
I hope it helps you.
Have a great day,
Radek
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Radek
Thank you for the support issue solved. But i am still not clear with mapping concept. How it works and how linking happens. If you dont mind can you please explain the concept.
Regards
Kiran Bhat
Hi Kiran,
Sure, it is really simple.
I will explain vector fetch on example.
When API interrupt occurs, the CPU finish current instruction and the interrupt module calculates offset according to interrupt source. In this case, it is 0x100.
See Table 1-13. Interrupt Vector Locations.
The CPU simply takes IVBR register content, move it to left by 8 bits (IVBR contains upper 15 bits from vector base address) and adds 0x100 offset. For example IVBR=0xFFC4. So, vector base is 0xFFC400. After adding 0x100 offset, we will get address 0xFFC500. At this address is stored starting address of API_ISR routine.
So, CPU will push their registers on stack and jump into API_ISR routine.
When code in API_ISR routine ends, the RTI instruction (Return from Interrupt) will pull back CPU registers from the stack.
Note: The RTI instruction is added on the end of ISR automatically because we used “interrupt” keyword in ISR declaration.
Note: Every vector has 4 bytes despite on fact that only 3 bytes are used for ISR address. So, if we want to fill a table with pointers to interrupt routines, we have to add dummy/padding byte at the beginning of every ISR address.
I hope it helps you.
Have a great day,
Radek
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------