Power consumption of a MM9Z1_638D1 at 125°C

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Power consumption of a MM9Z1_638D1 at 125°C

跳至解决方案
717 次查看
Boris_Bloxsberg
Contributor III

Hi,

 

has anyone experience with the power consumption of a MM9Z1_638D1  at 125°C. The data sheet says typ. 35mA at 85°C but whats about 125°C.

 

thanks

0 项奖励
1 解答
710 次查看
StanoA
NXP TechSupport
NXP TechSupport

Hello Boris,

There are no data measured on this limit temperature. But if you need define the current consumption limit for the application or for the local power supply I suggest you to add at least about 30 – 40% of the value for 85°C. It is my experience from my design praxis.

Have a nice day.

Stano.

在原帖中查看解决方案

1 回复
711 次查看
StanoA
NXP TechSupport
NXP TechSupport

Hello Boris,

There are no data measured on this limit temperature. But if you need define the current consumption limit for the application or for the local power supply I suggest you to add at least about 30 – 40% of the value for 85°C. It is my experience from my design praxis.

Have a nice day.

Stano.