Power consumption of a MM9Z1_638D1 at 125°C

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Power consumption of a MM9Z1_638D1 at 125°C

Jump to solution
817 Views
Boris_Bloxsberg
Contributor III

Hi,

 

has anyone experience with the power consumption of a MM9Z1_638D1  at 125°C. The data sheet says typ. 35mA at 85°C but whats about 125°C.

 

thanks

0 Kudos
Reply
1 Solution
810 Views
StanoA
NXP TechSupport
NXP TechSupport

Hello Boris,

There are no data measured on this limit temperature. But if you need define the current consumption limit for the application or for the local power supply I suggest you to add at least about 30 – 40% of the value for 85°C. It is my experience from my design praxis.

Have a nice day.

Stano.

View solution in original post

1 Reply
811 Views
StanoA
NXP TechSupport
NXP TechSupport

Hello Boris,

There are no data measured on this limit temperature. But if you need define the current consumption limit for the application or for the local power supply I suggest you to add at least about 30 – 40% of the value for 85°C. It is my experience from my design praxis.

Have a nice day.

Stano.