Power consumption of a MM9Z1_638D1 at 125°C

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Power consumption of a MM9Z1_638D1 at 125°C

ソリューションへジャンプ
715件の閲覧回数
Boris_Bloxsberg
Contributor III

Hi,

 

has anyone experience with the power consumption of a MM9Z1_638D1  at 125°C. The data sheet says typ. 35mA at 85°C but whats about 125°C.

 

thanks

0 件の賞賛
1 解決策
708件の閲覧回数
StanoA
NXP TechSupport
NXP TechSupport

Hello Boris,

There are no data measured on this limit temperature. But if you need define the current consumption limit for the application or for the local power supply I suggest you to add at least about 30 – 40% of the value for 85°C. It is my experience from my design praxis.

Have a nice day.

Stano.

元の投稿で解決策を見る

1 返信
709件の閲覧回数
StanoA
NXP TechSupport
NXP TechSupport

Hello Boris,

There are no data measured on this limit temperature. But if you need define the current consumption limit for the application or for the local power supply I suggest you to add at least about 30 – 40% of the value for 85°C. It is my experience from my design praxis.

Have a nice day.

Stano.