Message Edited by Alban on 05-10-2006 01:42 PM
Hi mcgeeph,
The S12X family does not have support for J1850 - the S12D family has J1850 support. I'm sorry I can't comment on future plans here (your local rep can help you) but there is a family roadmap available here.
hi, steve
in hcs12 to debug is necesary bdm interface, but my question is, could my pc debug throug tx, rx ? what is necesary, tools,harware sofware. to made a master eslave sistems witch pc monitor remote in each mcu
thanks
joose2006
Message Edited by Steve on 05-22-200609:32 AM
Keep_Smiling_2 wrote:Well Gordon,I hope you're not just producing these for the automotive industry; we all know where that's going;-)
Thanks Gordon. You've done a great job supporting these devices and I'm very happy overall. Sometimes I have to work with non-Freescale chips and it's frustrating trying to get the kind of low level information I need from them. Also, you guys were the first ones to support single wire debugging (was this 1998, I don't remember when the first 68hc12 BDM came out), and now that some other chip makers are *finally* starting to do this, they're treating it as a proprietary technology and they're not giving out the details (this applies to 2 companies I know of and I've heard that others are doing this also).
I'd love to see the source released for d-bug12, but I understand if that can't be done. We're still much better off with Freescale than with the others.