Hi Aaron,
The correct code creates an instance of AS1_TComData and then the function takes the address of the instance as a argument. The wrong code creates only a pointer. But the pointer doesn't point anywhere.
Regards,
Daniel
Hi Daniel,
I try to use Event of AS1_OnRxChar. It can work fine in DEBUG mode. But it can not work in NORMAL mode (remove MULTILINK then power off/on my board).
P.S. Main() code can work fine in both (DEBUG/NORMAL) mode.
void AS1_OnRxChar(void)
{
AS1_TComData *ReceiveChar;
/* Write your code here ... */
AS1_RecvChar(ReceiveChar);
switch(*ReceiveChar)
{
case 'C':
Pin_DO3 = 1; // LED4 OFF
Pin_RCK_DoorLock = 0; // Door Lock (Lo Active)
setReg8(DDRS, 0xF3U);
break;
case 'O':
Pin_DO3 = 0;// LED4 ON
Pin_RCK_DoorUnlock = 0; // Door Unlock (Lo Active)
setReg8(DDRS, 0xF5U);
break;
default:
setReg8(DDRS, 0xF1U);
break;
}
return;
}
Hi, Daniel,
I resolved the issue. But, I don't know why.
The wrong code as follow:
AS1_TComData *ReceiveChar;
AS1_RecvChar(ReceiveChar);
switch(*ReceiveChar)
The correct code as follow:
AS1_TComData ReceiveChar;
AS1_RecvChar(&ReceiveChar);
switch(ReceiveChar)
Best Regards,
Aaron
Hi Aaron,
The correct code creates an instance of AS1_TComData and then the function takes the address of the instance as a argument. The wrong code creates only a pointer. But the pointer doesn't point anywhere.
Regards,
Daniel
Hi Daniel,
ZVL32-SCI-CW106 can work fine. Then, I modify SCI0 to SCI1 (ZVL32-SCI1-CW106 as attachment). It can work, too.
But, I got many error when I merge the SCI1.c & SCI1.h into my Processor Expert project(B0005_Test as attachment). I don't know how to solve the error.
Have any SCI (UART) example for Processor Expert?
Best Regards,
Aaron