Current specification of EVDD pin

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Current specification of EVDD pin

867 次查看
curious
Contributor I

Hello community,

I am using the EVDD pin of the S12ZVM to provide a 5V supply to an external sensor (Op-Amp). The sensor has a 100n bypass MLCCs in parallel to the supply pins. What is the maximum transient current and the maximum time for the EVDD pin during switch on? The 100n capacitor is being charged during the switch on and the current limit is apparently exceeded for a short period of time. Is it ok to filter the overcurrent protection during this switch on time? In steady state the current consumption is about 3mA.

 

Thank you.

0 项奖励
回复
1 回复

855 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hello Florian,

As the Absolute maximum ratings specified, the I_EVDD1 instantaneous current must not exceed 80mA.

danielmartynek_1-1600859620916.png

danielmartynek_2-1600859653645.png

Maximum allowed continuous current is 20mA.

danielmartynek_3-1600859742999.png

Regards,

Daniel

 

 

0 项奖励
回复