Can the S12XE be used with Codewarrior 10.6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can the S12XE be used with Codewarrior 10.6

813 Views
highlander
Contributor II

Can the S12XE Reference board be developed with Codewarrior 10.6?

If it can, where can one download the jar package for the processor?


Thanks

0 Kudos
Reply
1 Reply

794 Views
lama
NXP TechSupport
NXP TechSupport

Hi,

CodeWarrior 1.6 Eclipse version was was designed for Magni V devices from S12 devices family.
CodeWarrior v 5.2 is the last version from the Classic type of CodeWarrior and support S12X family as a last family of the devices. Unfortunately, the version 5.2 does not contain files for ilder families of S12 family devices so if they are required they must be additionally inserted by procedure which can be found at our community pages. But this is not necessary for the device you use.
(https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/How-to-Add-missing-derivatives-to-CodeWarrio...)

Best regards,
Ladislav