I want to download the attachment from NXP RAPID-IOT-KIT EXAMPLES PROJECTS. However, the system says This file contains a virus or malware. The file has been deleted.
.
Can you upload the source code to GitHub instead? It would also be beneficial to read the code without downloading.
已解决! 转到解答。
Upload did not work corectly, sorry for that. Please find the source code on that repo:
GitHub - theophieleroy/rapid_iot_mcuxpresso_examples
Regards,
Upload did not work corectly, sorry for that. Please find the source code on that repo:
GitHub - theophieleroy/rapid_iot_mcuxpresso_examples
Regards,
The GitHub link works!
My experience so far (commit a1abcc96b1fca33caee172b31eb09d93e288c0bd):
When I import the project, a dialog appears:
After confirming the active selection (there are no other selections), the import completes. Question: is this warning harmful?
When I click Build in Quickstart Panel, the console shows this error*** No rule to make target 'C://_sdk_work/repo-directory/iot-rpk/utilities/fsl_assert.c', needed by 'utilities/fsl_assert.o'.
I grep'ed for _sdk_work
and found a reference in boards/rapidiotk64f/demo_apps/ble_sensors/.project
. In this file under /projectDescription/variableList
key, I changed both value
to $%7BPARENT-4-PROJECT_LOC%7D
, and the code compiles.
Uploading boards/rapidiotk64f/demo_apps/ble_sensors/Debug/ble_sensors.bin
to the kit works.
The problem is NOT SOLVED.
The downloaded ZIP file is INCOMPLETE and does not have the described examples. It contains a __All_Errors.txt
file that says:
Some files weren't downloaded. The limit of file downloads has been reached. The total number of file downloads cannot be greater than 200
When I download the RAPID-IOT_EXAMPLES.zip file I also get an error file that says: "Some files weren't downloaded. The limit of file downloads has been reached. The total number of file downloads cannot be greater than 200". When I go to import the examples the instructions do not match what I see in the IDE Import Projects from File System form. I am using IDE v10.3.0. I also cannot see the examples that are listed in your post.