nfs boot failure

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

nfs boot failure

1,525件の閲覧回数
pete1
Contributor I
I am trying to boot a P3041DS over NFS, but got this failure. Please help. Complete boot log is attached. The host PC is running SUSE 12.1.

---

IP-Config: Complete:
  device=eth3, addr=192.168.0.61, mask=255.255.255.0, gw=192.168.0.1,
  host=pz-nfs, domain=, nis-domain=(none),
  bootserver=192.168.0.106, rootserver=192.168.0.106, rootpath=
md: Skipping autodetection of RAID arrays. (raid=autodetect will force)
VFS: Mounted root (nfs filesystem) on device 0:15.
Freeing unused kernel memory: 288k freed
Installing knfsd (copyright (C) 1996 okir@monad.swb.de).
svc: failed to register nfsdv2 RPC service (errno 111).
nfsd: last server has exited, flushing export cache

---
0 件の賞賛
返信
3 返答(返信)

1,218件の閲覧回数
mattsm
Contributor III

Does NFS root work for other devices?

0 件の賞賛
返信

1,218件の閲覧回数
pete1
Contributor I

I am able to boot over NFS with an ubuntu 10.04 server.

Regards,

Peter Hua

Innovative Integration

0 件の賞賛
返信

1,218件の閲覧回数
mattsm
Contributor III

What NFS server are you using? How is it configured?

0 件の賞賛
返信