ls1012a GPIOs control by U-boot

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ls1012a GPIOs control by U-boot

3,580件の閲覧回数
nattapongsungch
Contributor III

Hi , 

 

I'm try to control GPIOs from U-boot. 

I found gpio control code from ../ls1012afrdm/eth.c  function name reset_phy() that used for reset PHY.

Then , I try to add more MASK bit to control GPIO1[16 :19] and enable GPIO1 on RCW.

 

Changing 

#define MASK_ETH_PHY_RST 0x00000100   -->  0x000F0100         

 

 

 

And I added debug print to read value that was set at DATA register looking it's doesn't change.

 

Clock Configuration:
CPU0(A53):800 MHz
Bus: 250 MHz DDR: 1000 MT/s
Reset Configuration Word (RCW):
00000000: 08000008 00000000 00000000 00000000
00000010: 35080000 c000000c 40000000 00001800
00000020: 00000000 00000000 00000000 00014171
00000030: 00000000 18c28120 00000096 00000000
I2C: ready
DRAM: 1022 MiB
SEC: RNG instantiated
Using SERDES1 Protocol: 13576 (0x3508)
MMC: FSL_SDHC: 0, FSL_SDHC: 1
SF: Detected S25FS512S_256K with page size 512 Bytes, erase size 128 KiB, total 64 MiB
PCIe1: Root Complex no link, regs @ 0x3400000
In: serial
Out: serial
Err: serial
Model: LS1012A RDB Board
Board: LS1012ARDB Version: RevB, boot from QSPI: bank1
SATA link 0 timeout.
AHCI 0001.0301 32 slots 1 ports 6 Gbps 0x1 impl SATA mode
flags: 64bit ncq pm clo only pmp fbss pio slum part ccc apst
Found 0 device(s).
SCSI: Net:
############# RESET PHY ###########
gpdat = 0001f000

###################################

 

 

 

Thank you,

Nattapong

Original Attachment has been moved to: eth.c.zip

16 返答(返信)

2,884件の閲覧回数
justinjonas
Contributor III

Chapter 19 of the reference manual for the LS1012A gives a list of all of the GPIO pins that are output only, input only, or reserved. The pins that that did not read back the correct value happened because the pin is an output only port. This implies that read modify write will not work with the output only pins.

0 件の賞賛
返信

2,884件の閲覧回数
justinjonas
Contributor III

Was this ever resolved? I am having the same issue.

0 件の賞賛
返信

2,884件の閲覧回数
nattapongsungch
Contributor III

Hi ,  Justin

Seem like register not changed when read back , but it is working.

0 件の賞賛
返信

2,884件の閲覧回数
ufedor
NXP Employee
NXP Employee

Please use U-Boot to check that the GPIO1 registers are configured properly.

Also try to write data to the corresponding DAT register.

2,884件の閲覧回数
nattapongsungch
Contributor III

Look like it's not changing at 0x2300008

=> md 2300000
02300000: 00010f00 00000000 00000100 00000100 ................
02300010: 00000000 00000000 00000000 00000000 ................
02300020: 00000000 00000000 00000000 00000000 ................
02300030: 00000000 00000000 00000000 00000000 ................
02300040: 00000000 00000000 00000000 00000000 ................
02300050: 00000000 00000000 00000000 00000000 ................
02300060: 00000000 00000000 00000000 00000000 ................
02300070: 00000000 00000000 00000000 00000000 ................
02300080: 00000000 00000000 00000000 00000000 ................
02300090: 00000000 00000000 00000000 00000000 ................
023000a0: 00000000 00000000 00000000 00000000 ................
023000b0: 00000000 00000000 00000000 00000000 ................
023000c0: 00000000 00000000 00000000 00000000 ................
023000d0: 00000000 00000000 00000000 00000000 ................
023000e0: 00000000 00000000 00000000 00000000 ................
023000f0: 00000000 00000000 00000000 00000000 ................
=> mw 2300000 ffffffff
=> md 2300000
02300000: ffffffff 00000000 00000100 00000100 ................
02300010: 00000000 00000000 00000000 00000000 ................
02300020: 00000000 00000000 00000000 00000000 ................
02300030: 00000000 00000000 00000000 00000000 ................
02300040: 00000000 00000000 00000000 00000000 ................
02300050: 00000000 00000000 00000000 00000000 ................
02300060: 00000000 00000000 00000000 00000000 ................
02300070: 00000000 00000000 00000000 00000000 ................
02300080: 00000000 00000000 00000000 00000000 ................
02300090: 00000000 00000000 00000000 00000000 ................
023000a0: 00000000 00000000 00000000 00000000 ................
023000b0: 00000000 00000000 00000000 00000000 ................
023000c0: 00000000 00000000 00000000 00000000 ................
023000d0: 00000000 00000000 00000000 00000000 ................
023000e0: 00000000 00000000 00000000 00000000 ................
023000f0: 00000000 00000000 00000000 00000000 ................
=> mw 2300008 ffffffff
=> md 2300000
02300000: ffffffff 00000000 00f00100 00f00100 ................
02300010: 00000000 00000000 00000000 00000000 ................
02300020: 00000000 00000000 00000000 00000000 ................
02300030: 00000000 00000000 00000000 00000000 ................
02300040: 00000000 00000000 00000000 00000000 ................
02300050: 00000000 00000000 00000000 00000000 ................
02300060: 00000000 00000000 00000000 00000000 ................
02300070: 00000000 00000000 00000000 00000000 ................
02300080: 00000000 00000000 00000000 00000000 ................
02300090: 00000000 00000000 00000000 00000000 ................
023000a0: 00000000 00000000 00000000 00000000 ................
023000b0: 00000000 00000000 00000000 00000000 ................
023000c0: 00000000 00000000 00000000 00000000 ................
023000d0: 00000000 00000000 00000000 00000000 ................
023000e0: 00000000 00000000 00000000 00000000 ................
023000f0: 00000000 00000000 00000000 00000000 ................
=> mw 2300008 00000000
=> md 2300000
02300000: ffffffff 00000000 00000000 00f00100 ................
02300010: 00000000 00000000 00000000 00000000 ................
02300020: 00000000 00000000 00000000 00000000 ................
02300030: 00000000 00000000 00000000 00000000 ................
02300040: 00000000 00000000 00000000 00000000 ................
02300050: 00000000 00000000 00000000 00000000 ................
02300060: 00000000 00000000 00000000 00000000 ................
02300070: 00000000 00000000 00000000 00000000 ................
02300080: 00000000 00000000 00000000 00000000 ................
02300090: 00000000 00000000 00000000 00000000 ................
023000a0: 00000000 00000000 00000000 00000000 ................
023000b0: 00000000 00000000 00000000 00000000 ................
023000c0: 00000000 00000000 00000000 00000000 ................
023000d0: 00000000 00000000 00000000 00000000 ................
023000e0: 00000000 00000000 00000000 00000000 ................
023000f0: 00000000 00000000 00000000 00000000 ................
=>

0 件の賞賛
返信

2,884件の閲覧回数
ufedor
NXP Employee
NXP Employee

In the provided log:

> => mw 2300008 ffffffff
> => md 2300000
> 02300000: ffffffff 00000000 00f00100 00f00100 ................

> => mw 2300008 00000000
> => md 2300000
> 02300000: ffffffff 00000000 00000000 00f00100 ................

> Look like it's not changing at 0x2300008

Not clear what do you mean.

0 件の賞賛
返信

2,884件の閲覧回数
nattapongsungch
Contributor III

Hi ufedor, 

> => mw 2300008 ffffffff
> => md 2300000
> 02300000: ffffffff 00000000 00f00100 00f00100 ................

0x00f00100 should be 0xffffffff. Why it was changed only byte number 7 and first bit  at byte number 2.

Thank you,

Nattapong

0 件の賞賛
返信

2,884件の閲覧回数
ufedor
NXP Employee
NXP Employee

> 0x00f00100 should be 0xffffffff.

Only GPIO signals' bits configured as outputs will be set to "1".

0 件の賞賛
返信

2,884件の閲覧回数
nattapongsungch
Contributor III

Yes, I also set all pin to output. by

=> mw 2300000 ffffffff

0 件の賞賛
返信

2,884件の閲覧回数
ufedor
NXP Employee
NXP Employee

Only pins configured as GPIO in the RCW are affected.

0 件の賞賛
返信

2,884件の閲覧回数
nattapongsungch
Contributor III

Yes, You are right. 

But , I changed SDHC1_BASE to GPIOs

0 件の賞賛
返信

2,884件の閲覧回数
ufedor
NXP Employee
NXP Employee

The RCW[SDHC1_BASE]  controls GPIO1[15:20].

0 件の賞賛
返信

2,884件の閲覧回数
ufedor
NXP Employee
NXP Employee

What is the RCW source?

0 件の賞賛
返信

2,884件の閲覧回数
nattapongsungch
Contributor III

Hello ufedor,

I'm using QCVS import PBL_0x35_0x08_800_250_1000_default.bin from LS1012A-SDK-AARCH64-IMAGE-20160830-yocto/ls1012ardb/

And change SDHC1_VSEL is GPIO and SDHC1_BASE are GPIOs.

rcw.png

Thank you,

Nattapong

0 件の賞賛
返信

2,884件の閲覧回数
ufedor
NXP Employee
NXP Employee

Have you configured the GPIO direction?

0 件の賞賛
返信

2,884件の閲覧回数
nattapongsungch
Contributor III

Yes, 

As I already attached eth.c

#define MASK_ETH_PHY_RST 0x000F0100

unsigned int val;
ccsr_gpio_t *pgpio = (void *)(CONFIG_SYS_GPIO1_ADDR);


setbits_be32(&pgpio->gpdir, MASK_ETH_PHY_RST);

.......

Thank you,

Nattapong

0 件の賞賛
返信