Transfer files to Linux system running on target from host Windows10 machine

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Transfer files to Linux system running on target from host Windows10 machine

1,290件の閲覧回数
pratik_vadher
Contributor II

I am using T1024RDB board with linux 3.12 from SDK 1.7. I am able to set the ip addresses and ping it from windows. I want to transfer files to Linux system. How do I do that via ethernet network? I tried using WinSCP but I get the error "Connection Refused". With FTP protocol, I get "No connection could be made because the target machine actively refused it. Connection failed."

タグ(1)
0 件の賞賛
返信
1 返信

1,244件の閲覧回数
Pavel
NXP Employee
NXP Employee

Linux on the T1024RDB supports TFTP communications.

See the following pages for TFTP using under Windows 10:

https://www.webservertalk.com/setup-configure-tftp-on-windows-10/

 

https://www.thewindowsclub.com/enable-tftp-windows-10

 

https://teckangaroo.com/enable-tftp-windows-10/

Have a great day,
Pavel Chubakov

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信