I'm trying to toggle gpio3_31 pin through sysfs in the ls1021atwr board.
I tried export 1 > gpio47/value
but the value remains 0, do I need to change the rcw configuration in u-boot?
this is the ls102xa_rcw_sd_ifc.cfg file
#PBL preamble and RCW header
aa55aa55 01ee0100
#enable IFC, disable QSPI and DSPI
0608000a 00000000 00000000 00000000
30000000 00007900 60040a00 21046000
00000000 00000000 00000000 20000000
00080000 881b7340 00000000 00000000
I'd like to modify the rcw image without using codewarrior can you please suggest which field to modify and what value to be added
解決済! 解決策の投稿を見る。
Please configure RCW[EC3] (422-424) as 001.
Please refer to the following from LS1021A Reference Manual.
Please configure RCW[EC3] (422-424) as 001.
Please refer to the following from LS1021A Reference Manual.