TWR-LS1021A:SDKv1.7 Sound card not detecting when booting linux via SDCARD.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

TWR-LS1021A:SDKv1.7 Sound card not detecting when booting linux via SDCARD.

1,414件の閲覧回数
khandavalli
Contributor I

Hi,

while trying to boot linux via sdcard, sound card is not getting detected, where as the same kernel when booted via NOR is getting detected without any issues. Followed instructions provided in QorIQ SDK 1.7 Documentation > Linux Kernel Drivers > Audio SAI section to enable Soundcard

Scenario1 Log Snippet (u-boot from NOR flash):

sgtl5000 1-000a: sgtl5000 revision 0x11

mmc0: new high speed SDHC card at address aaaa

sgtl5000 1-000a: Failed to get supply 'VDDD': -19

mmcblk0: mmc0:aaaa SU08G 7.40 GiB

1-000a: 1200 mV normal

sgtl5000 1-000a: Using internal LDO instead of VDDD

mmcblk0: p1 p2

vf610-sgtl5000 sound.9:  sgtl5000 <-> 2b50000.sai mapping ok ()

oprofile: using timer interrupt.

TCP: cubic registered

Initializing XFRM netlink socket

NET: Registered protocol family 17

NET: Registered protocol family 15

can: controller area network core (rev 20120528 abi 9)

NET: Registered protocol family 29

can: raw protocol (rev 20120528)

Key type dns_resolver registered

regulator-dummy: disabling

drivers/rtc/hctosys.c: unable to open rtc device (rtc0)

ALSA device list:

  #0: FSL-VF610-TWR-BOARD


Scenario2 (u-boot from SDCARD, same kernel)

sgtl5000: probe of 1-000a failed with error -110

vf610-sgtl5000 sound.9: ASoC: CODEC (null) not registered

vf610-sgtl5000 sound.9: TWR-AUDIO-SGTL board required :-517

platform sound.9: Driver vf610-sgtl5000 requests probe deferral

can: controller area network core (rev 20120528 abi 9)

NET: Registered protocol family 29

can: raw protocol (rev 20120528)

Key type dns_resolver registered

regulator-dummy: disabling

vf610-sgtl5000 sound.9: ASoC: CODEC (null) not registered

vf610-sgtl5000 sound.9: TWR-AUDIO-SGTL board required :-517

platform sound.9: Driver vf610-sgtl5000 requests probe deferral

ALSA device list:

  No soundcards found.


Are there any clock or regulator settings to be made in u-boot or have to be passed when using bootloader from the SDCARD?


0 件の賞賛
3 返答(返信)

1,004件の閲覧回数
sinanakman
Senior Contributor III

Hi Khandavalli

Can you compare RCW[SYS_PLL_CFG]  and RCW[SYS_PLL_RAT]

values in two RCWs you are using for the case of NOR boot and

SDCARD boot.

Regards

Sinan Akman

0 件の賞賛

1,004件の閲覧回数
khandavalli
Contributor I

Hi,

RCW{SYS_PLL_RAT} is 3 incase of NOR and RCW{SYS_PLL_CFG} is not availabe. Im using u-boot-spl-pbl for SDCARD which seems to be combination of RCW+pbl+u-boot. can you please let me know how can we check the values of SYS_PLL_RAT  in this case.

Im using 2014.07 u-boot.

Regards,

Arun

0 件の賞賛

1,004件の閲覧回数
sinanakman
Senior Contributor III

Hi Arun

I don't know why you mention some of the RCW values (e.g. RCW{SYS_PLL_CFG})  are not available.

I use mainline u-boot and not the SDK. I recommend you use mainline u-boot

as well. TWR-LS1021 is supported. The latest mainline u-boot shows the

RCW values during boot up. Here is what I see on my board with mainline

u-boot :

Booting from SD :

-----------------------

U-Boot 2015.01-00293-gb56f6e2 (Jan 21 2015 - 21:24:19)

CPU:   Freescale LayerScape LS1021E, Version: 1.0, (0x87081110)

Clock Configuration:                                                           

       CPU0(ARMV7):1000 MHz,                                                   

       Bus:300  MHz, DDR:800  MHz (1600 MT/s data rate),                       

Reset Configuration Word (RCW):                                                

       00000000: 0608000a 00000000 00000000 00000000                           

       00000010: 20000000 00407900 60040a00 21046000                           

       00000020: 00000000 00000000 00000000 00038000                           

       00000030: 00080000 881b7340 00000000 00000000

Booting fro NOR :

-----------------------

U-Boot 2015.01-00293-gb56f6e2-dirty (Jan 23 2015 - 00:25:40)

                                                                               

CPU:   Freescale LayerScape LS1021E, Version: 1.0, (0x87081110)                

Clock Configuration:                                                           

       CPU0(ARMV7):1000 MHz,                                                   

       Bus:300  MHz, DDR:800  MHz (1600 MT/s data rate),                       

Reset Configuration Word (RCW):

       00000000: 0608000a 00000000 00000000 00000000

       00000010: 70000000 00407900 e0025a00 21046000

       00000020: 00000000 00000000 00000000 00038000

       00000030: 00080000 881b7340 00000000 00000000

So perhaps you can just give mainline u-boot a try. I am not

familiar with SDKs and I personally prefer we all work out

of mainline u-boot. Let me know if you need further help

with this.

Regards

Sinan Akman

0 件の賞賛