Issue with SSL_Connect on QEMU

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Issue with SSL_Connect on QEMU

1,817 Views
navindaga
Contributor I

I'm using QorIQ Linux SDK v1.6 which has openssl version 1.0.1g. The host OS is CentOS 7.

I run QEMU emulation using qemu-system-ppc64 and I have not been able to establish SSL connection to a server. SSL Connection works from the host system but does not work on QEMU.

Any suggestions?

I use openssl s_client to test connection to the server and on QEMU, it reports :

"error:140790E5:SSL routines:SSL23_WRITE:ssl handshake failure:s23_lib.c:177:"

0 Kudos
Reply
1 Reply

1,681 Views
navindaga
Contributor I

Any thoughts anybody?

0 Kudos
Reply