T4240: DDR: What is the different between tWTR and WRT?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

T4240: DDR: What is the different between tWTR and WRT?

902件の閲覧回数
carlpeng
Contributor II

In the T4240RM.pdf, can find two register DDRx_TIMING_CFG_1[WRTORD], DDRx_TIMING_CFG_4[WRT], it seems the same, what is the difference?

0 件の賞賛
返信
1 返信

705件の閲覧回数
Bulat
NXP Employee
NXP Employee

Actually you could notice that descriptions of DDRx_TIMING_CFG_1[WRTORD] and DDRx_TIMING_CFG_4[WRT] are a bit different.

Basically the rule is as following, the DDR controlller automatically calculates time between WRITE and READ commands to meet tWTR (WRTORD) specification if READ hits the same memory bank (same CS). DDRx_TIMING_CFG_4[WRT] defines how many extra clock cycles will be added to that time. We recommnd to set this field to 0, i.e. default. This means that DDRx_TIMING_CFG_0[WRT] defines number of extra clock cycles. In turn we also recommend to set DDRx_TIMING_CFG_0[WRT] = 0, this will provide the fastest write-to-read turnaround timing.

Regards,

Bulat

0 件の賞賛
返信