Hi everybody,
I am designing a node based on T2080 and I want to implement one 10Gb Ethernet port.
I read on T2080RDBPCUG.pdf document the following sentence: "The T2080 only supports evaluation of the XFI protocol using Aquantia AQ1202 dual port 10GBase-T PHY".
That means the T2080 only works using the Aquantia AQ1202 IC or it refers to XFI protocol where, for example, I can use other PHY IC manufacturer as such Marvell or Broadcom?
Thanks on advance.
Regards.
Have a great day,
You can use other PHY IC compatible with the XFI.
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------