T2080 XFI 10GBase-T port support

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

T2080 XFI 10GBase-T port support

878 Views
filemón
Contributor I

Hi everybody,

I am designing a node based on T2080 and I want to implement one 10Gb Ethernet port.

I read on T2080RDBPCUG.pdf document the following sentence: "The T2080 only supports evaluation of the XFI protocol using Aquantia AQ1202 dual port 10GBase-T PHY".

That means the T2080 only works using the Aquantia AQ1202 IC or it refers to XFI protocol where, for example, I can use other PHY IC manufacturer as such Marvell or Broadcom?

Thanks on advance.

Regards.

Tags (2)
0 Kudos
2 Replies

709 Views
r8070z
NXP Employee
NXP Employee


Have a great day,

You can use other PHY IC compatible with the XFI.

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos

709 Views
filemón
Contributor I

Thank you for your reply.

Regards

0 Kudos