T1024 initialization script not working

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

T1024 initialization script not working

1,331 次查看
veerendranathj
Contributor III

Initializing T1024 processor failing with below error....(attached the tcl script using for initialization)

 

cmdwin::eclipse::config hexprefix 0x

cmdwin::eclipse::config MemIdentifier v

cmdwin::eclipse::config MemWidth 32

cmdwin::eclipse::config MemAccess 32

cmdwin::eclipse::config MemSwap off

cmdwin::reg regPPCTLB1/L2MMU_CAM1 = 0x7000000A1C08000000000000FE00000000000000FE000001

failed on register write: L2MMU_CAM1

thread break: Stopped, 0x0, 0x0, cpuPowerPCBig,  Connected (state, tid, pid, cpu, target)

cmdwin::reg regPPCTLB1/L2MMU_CAM2 = 0x9000000A1C08000000000000400000000000000040000001

 

 

Original Attachment has been moved to: T1024_init_core.tcl.zip

0 项奖励
回复
5 回复数

992 次查看
addiyi
NXP Employee
NXP Employee

Try to attach to the board, then reset the board (using Reset button) without using an Initialize target script. Also, in ccs console, activate verbose log using "log v" command 

After that open Debugger Shell view and run the followings commands:

%>variable CAM_GROUP "regPPCTLB1/"
%>reg ${CAM_GROUP}L2MMU_CAM1
+ regPPCTLB1
L2MMU_CAM1=0x7000000A18080000FE00000000000000
%>reg ${CAM_GROUP}L2MMU_CAM1 =
0x7000000A1C08000000000000FE00000000000000FE000001
%>reg ${CAM_GROUP}L2MMU_CAM1
+ regPPCTLB1
L2MMU_CAM1=0x7000000A1C08000000000000FE00000000000000FE000001

Please provide the output from Debugger Shell view and from ccs console, and also attach the memory file used.

Also 

0 项奖励
回复

992 次查看
ufedor
NXP Employee
NXP Employee

Which board is in question?

0 项奖励
回复

992 次查看
veerendranathj
Contributor III

It's not evalboard.. Our product board.

0 项奖励
回复

992 次查看
ufedor
NXP Employee
NXP Employee

It is convemient to investigate complicated bring-up issues as Terchnical Cases:

https://community.freescale.com/thread/381898

0 项奖励
回复

992 次查看
veerendranathj
Contributor III

There is no issue in board bring up. We already completed board bring up we used Trace32 debugger to complete it. Here issue is similar initialization trace32 cmm script working fine when we use trace32 tool but code warrior tcl script not working as expected.

0 项奖励
回复