Hello,
According to QorIQ-SDK-2.0-1609-IC-Rev1.pdf, page 69, in order to change u-boot code:
3. $ cd <S>
Note: Use bitbake -e <package-name> | grep ^S= to get value of <S>, the package source code
directory.
I do not understand. What is <S> ?
Thank you,
Z.V
<S> is a pseudo-variable that receives the value of a string produced by the following pipe:
bitbake -e <package-name> | grep ^S=
Below is how it works on my machine:
$ bitbake -e u-boot | grep ^S=
S="/home/platon/private/ltib/QorIQ-SDK-V2.0-20160527-yocto/build_ls1043ardb/tmp/work/ls1043ardb-fsl-linux/u-boot-qoriq/2016.01+fslgit-r0/git"
$ cd /home/platon/private/ltib/QorIQ-SDK-V2.0-20160527-yocto/build_ls1043ardb/tmp/work/ls1043ardb-fsl-linux/u-boot-qoriq/2016.01+fslgit-r0/git
$ ls
api common disk dts include lib ls1043ardb_nand_config MAKEALL post snapshot.commit
arch config.mk doc examples Kbuild Licenses ls1043ardb_sdcard_config Makefile README test
board configs drivers fs Kconfig ls1043ardb_config MAINTAINERS net scripts tools
More information on bitbake command interface can be found here:
Have a great day,
Platon
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------