Question on circuit diagram Bill of Material for T2080-RDB

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Question on circuit diagram Bill of Material for T2080-RDB

815 次查看
takayukiyamazak
Contributor I

Hi NXP

I purchased T2080-RDB at NXP WEB.
RDB purchased as ECO development.

I need information in a hurry. please tell me.

I want to check the circuit diagram of this product. But there is not any document on the product.

There was no CDROM.

Where do I get the circuit diagram and parts list?

It is helpful to get information by e-mail.

Best regards

0 项奖励
回复
2 回复数

584 次查看
alexander_yakov
NXP Employee
NXP Employee

Board User Guide and schematic in PDF format should be available on USB stick with board documentation.

Board design sources (schematic in Orcad format, board layout, BOM and FPGA sources) are available for free, but under NDA. To sign NDA and get this confidential board collateral, please contact your distributor.

Distributor Network|NXP 


Have a great day,
Alexander

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

584 次查看
takayukiyamazak
Contributor I

Thank you for answering

I think that USB was not included.

I am trading with AVNET. I'll talk to AVNET

Best regards

--

Gigafirm co.,ltd.

山崎 隆行 yamazaki takayuki

e-mail:yamazaki.tk@gigafirm.com

http://www.gigafirm.com/

2017-02-14 1:06 GMT+09:00 alexander.yakovlev <admin@community.nxp.com>:

NXP Community

<https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>

Re: Question on circuit diagram Bill of Material for T2080-RDB

reply from alexander.yakovlev

<https://community.nxp.com/people/alexander.yakovlev?et=watches.email.thread>

in QorIQ Processing Platforms - View the full discussion

<https://community.nxp.com/message/876628?commentID=876628&et=watches.email.thread#comment-876628>

0 项奖励
回复