QorIQ T2080 Processor Power calculation/Estimation queries

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

QorIQ T2080 Processor Power calculation/Estimation queries

跳至解决方案
2,448 次查看
KLN
Contributor III

Hi,

We are going to use QorlQ T2080 Processor.

For Power calculation of the processor, Any excel/document is available to use?

Also, we are planning to use PCIe interface to NVMe SSD. As Processor will be root-complex and  SSD will be End nodes, End nodes to be powered up and should be up before the root-complex, Should power sequence need to be taken care or processor will handle this??

And Processor will be End-point in another use case. 

 

 

标签 (1)
标记 (2)
0 项奖励
回复
1 解答
2,259 次查看
mrudangshelat-13
NXP TechSupport
NXP TechSupport

Hi @KLN,

The required power sequencing is mentioned in the section# 3.2 of T2080 datasheet.

Regards,
Mrudang

在原帖中查看解决方案

0 项奖励
回复
9 回复数
2,432 次查看
mrudangshelat-13
NXP TechSupport
NXP TechSupport

Hi @KLN,

Refer to section# 3.4 in the T12080 datasheet and specifically table# 8 for T2080 I/O power dissipation.

Regards,
Mrudang

0 项奖励
回复
2,426 次查看
KLN
Contributor III

Hi @mrudangshelat-13 
I understand that Datasheet has mentioned power details in the datasheet.

I was specifically asking for the Excel is available for ease of use.

Also Please note that I have asked about SSD related question also.

0 项奖励
回复
2,391 次查看
mrudangshelat-13
NXP TechSupport
NXP TechSupport

Hi @KLN,

There is no such excel available.

Regarding the SSD related question, I am working on it and I will let you know once I have any findings.

Regards
Mrudang

0 项奖励
回复
2,385 次查看
KLN
Contributor III

Hi @mrudangshelat-13 

Thanks for your response.

Please let us know at the earliest. I do see that responses are very slow.

0 项奖励
回复
2,366 次查看
mrudangshelat-13
NXP TechSupport
NXP TechSupport

Hi @KLN,

I apologize for the delay as I was facing some server glitches since last week.

I would suggest to implement a power switching circuit for the powering up the end node in order to avoid unwanted voltage to processor(root complex) from the end node when end node is powered up before the processor.

Regards,
Mrudang

0 项奖励
回复
2,353 次查看
KLN
Contributor III

Hi @mrudangshelat-13 

Thanks for your response.

One more query on T2080 Evaluation board:

What is the purpose of connecting T2080's IFC to CPLD?

 

KLN_0-1676898179271.png

 

 

KLN_1-1676898266844.png

KLN_2-1676898424780.png

 

0 项奖励
回复
2,330 次查看
mrudangshelat-13
NXP TechSupport
NXP TechSupport

HI @KLN 

Kindly raise the new ticket for the additional queries.

Thanks,

Mrudang

0 项奖励
回复
2,320 次查看
KLN
Contributor III

One more query on T2080 Power related,

Are there any requirement of Sequencing of power?

0 项奖励
回复
2,260 次查看
mrudangshelat-13
NXP TechSupport
NXP TechSupport

Hi @KLN,

The required power sequencing is mentioned in the section# 3.2 of T2080 datasheet.

Regards,
Mrudang

0 项奖励
回复