QorIQ T2080 Processor Power calculation/Estimation queries

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

QorIQ T2080 Processor Power calculation/Estimation queries

Jump to solution
2,428 Views
KLN
Contributor III

Hi,

We are going to use QorlQ T2080 Processor.

For Power calculation of the processor, Any excel/document is available to use?

Also, we are planning to use PCIe interface to NVMe SSD. As Processor will be root-complex and  SSD will be End nodes, End nodes to be powered up and should be up before the root-complex, Should power sequence need to be taken care or processor will handle this??

And Processor will be End-point in another use case. 

 

 

Labels (1)
Tags (2)
0 Kudos
Reply
1 Solution
2,239 Views
mrudangshelat-13
NXP TechSupport
NXP TechSupport

Hi @KLN,

The required power sequencing is mentioned in the section# 3.2 of T2080 datasheet.

Regards,
Mrudang

View solution in original post

0 Kudos
Reply
9 Replies
2,412 Views
mrudangshelat-13
NXP TechSupport
NXP TechSupport

Hi @KLN,

Refer to section# 3.4 in the T12080 datasheet and specifically table# 8 for T2080 I/O power dissipation.

Regards,
Mrudang

0 Kudos
Reply
2,406 Views
KLN
Contributor III

Hi @mrudangshelat-13 
I understand that Datasheet has mentioned power details in the datasheet.

I was specifically asking for the Excel is available for ease of use.

Also Please note that I have asked about SSD related question also.

0 Kudos
Reply
2,371 Views
mrudangshelat-13
NXP TechSupport
NXP TechSupport

Hi @KLN,

There is no such excel available.

Regarding the SSD related question, I am working on it and I will let you know once I have any findings.

Regards
Mrudang

0 Kudos
Reply
2,365 Views
KLN
Contributor III

Hi @mrudangshelat-13 

Thanks for your response.

Please let us know at the earliest. I do see that responses are very slow.

0 Kudos
Reply
2,346 Views
mrudangshelat-13
NXP TechSupport
NXP TechSupport

Hi @KLN,

I apologize for the delay as I was facing some server glitches since last week.

I would suggest to implement a power switching circuit for the powering up the end node in order to avoid unwanted voltage to processor(root complex) from the end node when end node is powered up before the processor.

Regards,
Mrudang

0 Kudos
Reply
2,333 Views
KLN
Contributor III

Hi @mrudangshelat-13 

Thanks for your response.

One more query on T2080 Evaluation board:

What is the purpose of connecting T2080's IFC to CPLD?

 

KLN_0-1676898179271.png

 

 

KLN_1-1676898266844.png

KLN_2-1676898424780.png

 

0 Kudos
Reply
2,310 Views
mrudangshelat-13
NXP TechSupport
NXP TechSupport

HI @KLN 

Kindly raise the new ticket for the additional queries.

Thanks,

Mrudang

0 Kudos
Reply
2,300 Views
KLN
Contributor III

One more query on T2080 Power related,

Are there any requirement of Sequencing of power?

0 Kudos
Reply
2,240 Views
mrudangshelat-13
NXP TechSupport
NXP TechSupport

Hi @KLN,

The required power sequencing is mentioned in the section# 3.2 of T2080 datasheet.

Regards,
Mrudang

0 Kudos
Reply