Hi,
I got following error on running FMC:
cpu0: ! CRITICAL FM-PCD Error [CPU00, drivers/net/ethernet/freescale/fman/Peripherals/FM/Pcd/fm_pcd.c:1120 FM_PCD_Enable]: Invalid Handle;
cpu0: cpu0:
cpu0: ! MINOR FM Error [CPU00, drivers/net/ethernet/freescale/fman/src/wrapper/lnxwrp_ioctls_fm.c:3038 LnxwrpFmPcdIOCTL]: Invalid Handle;
cpu0: IOCTL FM PCDcpu0:
ERR : cpu0: ! CRITICAL FM-PCD Error [CPU00, drivers/net/ethernet/freescale/fman/Peripherals/FM/Pcd/fm_pcd.c:1176 FM_PCD_Disable]: Invalid Handle; Invocation of FM
cpu0: _PCD_Enable for cpu0:
fm0/pcd failed wcpu0: ! MINOR FM Error [CPU00, drivers/net/ethernet/freescale/fman/src/wrapper/lnxwrp_ioctls_fm.c:3038 LnxwrpFmPcdIOCTL]: Invalid Handle; ith error cod
e 0
cpu0: IOCTL FM PCDx00010013
cpu0:
ERR : Invocation of FM_PCD_Disable for fm0/pcd failed with error code 0x00010013
Any idea?
Hi M.Adeel Sharif,
I have one question here Have you tried doing ping from dis FRA application.
My setup of working is I am running this FRA on T4240rdb board . I am able to test the whole configuration with test_speed.c and pw.c but i am not able to test the setup with ARP and MAC binding ? If u have tried doing physical interfaces Please do guide me because i need this FRA to run on Ethernet interfaces. RMAN is working fine that i know and I am getting 28Gbps throughput through test speed performance test.
thanks
Loveleen
Hello M.Adeel Sharif,
Please make sure that you have specified the appropriate configuration and policy file, for P2041, please refer to the following.
# cd /usr/etc
# fmc -c usdpaa_config_p2_p3_p5_14g.xml -p usdpaa_policy_hash_ipv4.xml –a
Please provide more detailed information regarding your problem.
Which version Linux SDK are you using?
Which version target board are you using? P2041RDB-PB?
Would you please provide some steps to help me to reproduce your problem?
Have a great day,
Yiping
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Yiping,
The problem regarding FMC is solved. I am working on running FRA application. When I use 'fra_config_dstr_processing1.xml' distribution, I got the following output on FRA console:
fman_nonhash_dqrr receives a message fqid=0x57 fd_status = 0x00000000
drop: bpid 9 <-- 0x1cd7f940
Even if I send ping request from Host computer, I always see only this msg on FRA console. Do you know what this msg means? Also, how can I check if there is any msg received by the RMAN at all?
Thanks and Regards
Adeel
Hello M.Adeel Sharif,
Please send your console log to me, including u-boot and whole Linux system logs, I will do more investigation for you.
Thanks,
Yiping
Hi Yiping,
The above problem regarding the 'fman_nonhash_dqrr' message is also solved :smileyhappy: Could you please check if there is any TX/RX counters in RMAN? I mean how can I check if RMAN really transmits something? The other endpoint is SRIO switch and I saw no RX counter on P2041 SRIO port. One more thing how to do enumeration and discovery using USDPAA application as it has been done before by Kernel drivers?
Thanks and regards,
Adeel
Hello M.Adeel Sharif,
There is no hardware statistics mechanism in RMAN. In USDPAA FRA application, there is a demo named "test_speed", probably it is useful for you to do some counting work, this demo simulates RMAN to RMAN communication directly. When launching FRA application, you could use configuration file fra_config_dstr_testspeed_rxpoint.xml and fra_config_dstr_testspeed_txpoint.xml.
usage in fra>
testspeed [send/receive] [packet length] [packet number] [loop number]
USDPAA FRA application invokes USDPAA RMAN driver APIs provided in USDPAA packages.
Thanks,
Yiping
Hi Yiping,
Thanks for your support. I have tried testspeed and it is showing speed for mailbox, streaming and doorbell. Could you explain a bit about how it measures those speed? For instance in send mode, it queues some frame in queue manager and in the end shows time taken by the test. How did it calculate this time interval?
One important thing is how to do enumeration and discovery using USDPAA application as it has been done before by Kernel drivers?
Thanks and regards,
Adeel
Hello Adeel,
Please refer to the attached source file from USDPAA package.
Please refer to “test_speed_to_send” in main.c and "test_speed_wait_receive“ function in test_speed.c
Have a great day,
Yiping
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------