P2020RDB vs P2020DS

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

P2020RDB vs P2020DS

946 次查看
leventozturk
Contributor I

What is the difference between P2020RDB and P2020DS other than number of Ethernet ports and memory sizes? Which one is more functional?

0 项奖励
回复
2 回复数

795 次查看
alexander_yakov
NXP Employee
NXP Employee

RDB board is usually positioned as low-cost, whereas DS board is typically full-featured.

For P2020 processor you can look both board photos on our web to see the difference.

P2020DS

http://cache.freescale.com/files/graphic/block_diagram/P2020DS_BD.jpg

P2020RDB

http://cache.freescale.com/files/graphic/product_freescale/P2010RDB.jpg

Visible differences - DIMM slot for memory on DS board, two x16 PCI-E slots, one conventional PCI slot, slot for SGMII riser card, SATA connectors, SD card, USB connectors

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

795 次查看
leventozturk
Contributor I

P2020DS board specifications and block diagram shows 3 Ethernet port but I can see only one on the picture? Are there 3 or 1 physical ports on the P2020DS board?

0 项奖励
回复