LX2160A -

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LX2160A -

1,778 Views
james_l_thompso
Contributor I

On the LX2160A, is it possible to do MPLS L2 switching on the WRIOP alone (without A72 cores)?

If so, how is it enabled?

Tags (1)
0 Kudos
Reply
1 Reply

879 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello James Thompson ,

MC provides object(DPSW) which internally implements DPAA2 H/W Switch. This Switch instance can also be used
for traffic forwarding to multiple hosts. DPSW has its own filter table which populates dynamically with source MAC address and port which packet is received on. Default incoming traffic will be flooded to all ports except ingress port and filtering rules will be learnt into filtering table. After learning,same packet will be forwarded to the destined port only.

The DPDMUX is another type of switch. It differs from a DPSW in several ways. A DPDMUX may have only a single uplink port. Also, it can be programmed to direct packets based on header values above layer 2.


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply